EAGLE User Support (English) Easy job, need help, I am a hobbyist.
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 179 subscribers
  • Views 190 views
  • Users 0 members are here
  • scr
  • Experiment
  • help
  • thyristor
  • flash
Related

Easy job, need help, I am a hobbyist.

Former Member
Former Member over 10 years ago

So hello everyone, I hope I am posting this question to the right place. I am trying to make something based an a book I found, s small circuit (see image) that activates a flash when a loud sound is made, just like the clap thing that switches on and off the lights.  The flash I am using has batteries (starblitz 220 baz) and it flashes when the 2 terminals are conected (even if it connected for a couple of seconds it only flashes once). So the schematic I found makes me think that the Thyristor used is actually passing current through the flash and it makes me wonder if i could achieve the same result using a simple transistor. Any ideas?. If I decide to use a thyristor (and if this works okay with the flash and no current passing) is it a big problem that i can't find a 400V,6A SCR. I can only find 800V, 12A where I live. Your help will help a lot with a project that I am working on currently!

 

Project sheet

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 10 years ago +1
    Hi, The SCR with the 800 volt 12 A rating will substitute just fine for the 400 volt 6 amp one in this application. The transistor that you mention may not work as well as it may trigger the flash before…
Parents
  • jw0752
    0 jw0752 over 10 years ago

    Hi,

    The SCR with the 800 volt 12 A rating will substitute just fine for the 400 volt 6 amp one in this application. The transistor that you mention may not work as well as it may trigger the flash before or after the event. It probably wouldn't hurt to try it though. The SCR will trigger and stay latched until the power is removed while the transistor will turn on and off with each voltage spike that switches the OP Amp.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 10 years ago

    Hi,

    The SCR with the 800 volt 12 A rating will substitute just fine for the 400 volt 6 amp one in this application. The transistor that you mention may not work as well as it may trigger the flash before or after the event. It probably wouldn't hurt to try it though. The SCR will trigger and stay latched until the power is removed while the transistor will turn on and off with each voltage spike that switches the OP Amp.

    John