EAGLE User Support (English) Error messages during simulation with Eagle-PCBsim: timestep too small, iteration limit exceeded: what next?
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
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 178 subscribers
  • Views 610 views
  • Users 0 members are here
  • pcbsim
Related

Error messages during simulation with Eagle-PCBsim: timestep too small, iteration limit exceeded: what next?

Former Member
Former Member over 10 years ago

Using PCBsim in a circuit intended to produce fast changing voltages I often get errors: " timestep too small" or " iteration limit exceeded".

In one case this was cured by pulling up/down a certain net in the circuit to GND via 10k resistors.

However, pulling these nets to the rail voltages +/- 24 V via the same resistor again led to the errors.

 

This looks confusing to me.

How can one deal with such internal(?) PCBsim errors?

 

Thanks,

Jan

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 1/2/2016 3:32 AM, J Cuppen wrote:

    Using PCBsim in a circuit intended to produce fast changing voltages I

    often get errors: " timestep too small" or " iteration limit exceeded".

    In one case this was cured by pulling up/down a certain net in the

    circuit to GND via 10k resistors.

    However, pulling these nets to the rail voltages +/- 24 V via the same

    resistor again led to the errors.

     

    This looks confusing to me.

    How can one deal with such internal(?) PCBsim errors?

     

    Thanks,

    Jan

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/170491

     

    Hi Jan,

     

    I've contacted the developer of PCB Sim to see if he can jump into the

    forums to help.

     

    The issue you are describing sounds like a convergence issue. This is

    something common to all simulators where depending on the model and it's

    connections the equation solver used by the SPICE engine is unable to

    converge to a solution.

     

    If grounding via 10 resistors allowed for a solution and it doesn't make

    a practical difference in your physical circuit then I think those

    results could be acceptable.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to autodeskguest

    Hi Jorge, Thanks for your response.

     

    Yes, there must be convergence issues. The workaround described however works only very partially.

    Asking pcbsim to calculate power for a number of components in the circuit (with the resistors) again leads to the breakdown with tese error messages.

    So my question remains open and I would very much appreciate an answer from development.

     

    Kind Regards,

    Jan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to autodeskguest

    Hi Jorge, Thanks for your response.

     

    Yes, there must be convergence issues. The workaround described however works only very partially.

    Asking pcbsim to calculate power for a number of components in the circuit (with the resistors) again leads to the breakdown with tese error messages.

    So my question remains open and I would very much appreciate an answer from development.

     

    Kind Regards,

    Jan