Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How do you keep the Schematic Capture Grid Display Settings?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 1439 views
  • Users 0 members are here
Related

How do you keep the Schematic Capture Grid Display Settings?

COMPACT
COMPACT over 10 years ago

Hi Jorge,

 

With 7.5 how does one keep the schematic grid option set to how it was when the current schematic file was last opened?

 

If I open a Schematic, set grid display on, save the file, exit EAGLE and then restart EAGLE and open the schematic file the grid is now off.

 

Cheers

 

Compact

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 2/3/2016 3:51 PM, COMPACT wrote:

    Hi Jorge,

     

    With 7.5 how does one keep the schematic grid option set to how it was

    when the current schematic file was last opened?

     

    Hi Compact,

     

    The easiest way would be to set this up as a default in the eagle.scr

    file. Open the eagle.scr file (It's accesible from the Control Panel >

    Scripts tree). Find the SCH: heading.

     

    Beneath the SCH heading add the following line:

    GRID ON;

     

    Save the eagle.scr file. Now every time you open a schematic the grid

    will be visible. The eagle.scr file is very useful for setting up

    defaults since it runs every time a new editor is opened.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 10 years ago in reply to autodeskguest

    Thanks Jorge, but what about schematic files that I want the display grid to remain off when opened?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to COMPACT

    On 5/02/2016 8:59 a.m., COMPACT wrote:

    Thanks Jorge, but what about schematic files that I want the display

    grid to remain off when opened?

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/173576

     

     

     

    Changes need to be made in the same area of eagle.scr.

     

    Each board records the grid setting. When that board is opened the grid

    will be as you left it. But straight away after the schematic is opened,

    the file eagle.scr runs so you are left seeing what it sets.

     

    By default, eagle.scr will set the grid to default with the command

    grid default

    Look for the following in eagle.scr

     

    SCH:

    Grid Default;

     

    Now default is Grid off and 0.1inch. You can confirm this in the

    schematic editor by opening the grid dialogue and clicking 'default'

     

    So what you need to do is get rid of the "Grid Default;" line.

     

    Because it is somewhat compulsory to use a 0.1" grid I would make it all

    default except without the grid on or off part so the line would become

     

    GRID inch 0.1 1 lines alt inch 0.01;

     

    See the HELP about the GRID command for other options you may prefer to

    be forced by eagle.scr

     

    HTH

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    On 5/02/2016 9:39 p.m., Rob Pearce wrote:

    On 05/02/16 05:21, warrenbrayshaw wrote:

    So what you need to do is get rid of the "Grid Default;" line.

     

    Because it is somewhat compulsory to use a 0.1" grid I would make it all

    default except without the grid on or off part so the line would become

     

    GRID inch 0.1 1 lines alt inch 0.01;

     

    It should be possible to set that with:

    GRID default;

    GRID lines on;

     

    which may feel more intuitive for achieving what's needed.

     

     

    No, not at all.

    Compact wants the schematic saved value to control the visibility of the

    grid so the eagle.scr cannot contain anything that controls grid visibility.

     

    Both your commands force visibility. First off and then on

     

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    On 5/02/2016 9:39 p.m., Rob Pearce wrote:

    On 05/02/16 05:21, warrenbrayshaw wrote:

    So what you need to do is get rid of the "Grid Default;" line.

     

    Because it is somewhat compulsory to use a 0.1" grid I would make it all

    default except without the grid on or off part so the line would become

     

    GRID inch 0.1 1 lines alt inch 0.01;

     

    It should be possible to set that with:

    GRID default;

    GRID lines on;

     

    which may feel more intuitive for achieving what's needed.

     

     

    No, not at all.

    Compact wants the schematic saved value to control the visibility of the

    grid so the eagle.scr cannot contain anything that controls grid visibility.

     

    Both your commands force visibility. First off and then on

     

    Warren