Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Tidy schematic after pinswap
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 191 subscribers
  • Views 2555 views
  • Users 0 members are here
  • pinswap schematic
Related

Tidy schematic after pinswap

alberthall
alberthall over 10 years ago

I am working on a design using a microcontroller using analogue inputs and digital I/O.   The analogue pins can be swapped and the digital pins can be swapped at will (with commensurate changes in the firmware).  I have set the swap levels on the part to allow this.  I put short wires on each pin and named them and did likewise with the parts they connected to.  The parts on the board layout are connected correctly but the layout would be better if some pins were swapped.   So, on the schematic I swap some pins and the board layout correctly reflects the changes.   The problem is that the schematic is now a mess wire wires draped all over the microcontroller.  I tried using Bus/Net but the result is similar.

 

Is there a way of using pinswap without making a mess of the schematic?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    James Thurgood wrote on Sat, 06 February 2016 09:07

    Is there a way of using pinswap without making a mess of the schematic?

     

     

    Stop and actually think about it.  How do you expect this to work?  Laying

    out a schematic to be nicely readable requires much higher level judgement

    above the mere connection topology Eagle knows about.  This isn't going to

    work for the same reason Eagle doesn't have some automatic "beautify"

    function for the schematic.  Too much high level knowledge and artistic

    judgement is required to do anything useful, not to mention the algorithms

    would be very complex even if this were possible somehow.

     

    It will continue to be your job to draw a clear schematic for the

    reasonably forseable future.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    Olin Lathrop wrote:

     

    James Thurgood wrote on Sat, 06 February 2016 09:07

    Is there a way of using pinswap without making a mess of the schematic?

     

    Stop and actually think about it.  How do you expect this to work?  Laying

    out a schematic to be nicely readable requires much higher level judgement

    above the mere connection topology Eagle knows about.

     

    Why? To swap two equivalent pins on the board you only have to change the

    pin number in the schematic, nothing has to be redrawn (otherwise the pins

    were not swapable in the first place).

     

    Gruss, Matthias Dingeldein

     

    --

    Guillotinen sind nicht reziprok, aber das macht nix,

    die werden eh nur fuer die Hinrichtung verwendet

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    On 06/02/16 15:59, Matthias Dingeldein wrote:

    Why? To swap two equivalent pins on the board you only have to change the

    pin number in the schematic, nothing has to be redrawn (otherwise the pins

    were not swapable in the first place).

     

    But to swap pin numbers in the schematic **FUNDAMENTALLY CHANGES THE

    DEVICE** and is thus absolutely not an option. It may work for many

    cases - the simple logic gates could be mirrored in an appropriate axis,

    if there were a predictable way to identify that axis - but not in the

    general case. Specifically, in the case that the OP asked about, he is

    swapping pins of a micro. Thus your "just swap the pin numbers" idea

    would result in two port pins being wrongly allocated. That's FAR WORSE

    than the mess that currently needs cleaning up.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    On 07/02/16 10:25, Matthias Dingeldein wrote:

    If the pins are not equivalent, your idea is the best way to handle it, but

    in case of logic gates (for example) I can't see any reason why "just

    renumbering" might cause any trouble

     

    The problem is that you're looking at a (potentially small) subset of

    cases and saying "my way works for these, so it's good". That's very bad

    logic. You can't extrapolate from the specific to the general in a

    positive sense. I'm saying "here are some cases where it doesn't work",

    which is sufficient to exclude it as a general solution. Now, perhaps,

    it might be of limited use as a user-triggered "tidy-up" option, but I

    suspect the extra overhead of maintaining the ability to arbitrarily

    swap pin numbers within a schematic symbol (which, I should point out,

    is NOT SOMETHING EAGLE CAN DO at the moment, for generally good reason)

    would be worth it. Especially as, due to the existence of cases where

    it's blatantly wrong, there would need to be an extra layer of "allow

    this to be done" conditions in the library component definition.

     

    Besides, for the bulk of your cases (logic gates) it's already quite

    easy for the user to tidy up with a combination of mirror and rotate.

     

    And, apparently unlike you, I positively detest schematics which show

    the pin-out order from the arbitrary package (which is often different

    between SSOP and TQFP anyway) in preference to the logical pin ordering

    that functionality implies. My CPU parts are ALL shown on the schematic

    with the port pins in bit number order.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    On 07/02/16 10:25, Matthias Dingeldein wrote:

    If the pins are not equivalent, your idea is the best way to handle it, but

    in case of logic gates (for example) I can't see any reason why "just

    renumbering" might cause any trouble

     

    The problem is that you're looking at a (potentially small) subset of

    cases and saying "my way works for these, so it's good". That's very bad

    logic. You can't extrapolate from the specific to the general in a

    positive sense. I'm saying "here are some cases where it doesn't work",

    which is sufficient to exclude it as a general solution. Now, perhaps,

    it might be of limited use as a user-triggered "tidy-up" option, but I

    suspect the extra overhead of maintaining the ability to arbitrarily

    swap pin numbers within a schematic symbol (which, I should point out,

    is NOT SOMETHING EAGLE CAN DO at the moment, for generally good reason)

    would be worth it. Especially as, due to the existence of cases where

    it's blatantly wrong, there would need to be an extra layer of "allow

    this to be done" conditions in the library component definition.

     

    Besides, for the bulk of your cases (logic gates) it's already quite

    easy for the user to tidy up with a combination of mirror and rotate.

     

    And, apparently unlike you, I positively detest schematics which show

    the pin-out order from the arbitrary package (which is often different

    between SSOP and TQFP anyway) in preference to the logical pin ordering

    that functionality implies. My CPU parts are ALL shown on the schematic

    with the port pins in bit number order.