Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Tidy schematic after pinswap
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 191 subscribers
  • Views 2433 views
  • Users 0 members are here
  • pinswap schematic
Related

Tidy schematic after pinswap

alberthall
alberthall over 10 years ago

I am working on a design using a microcontroller using analogue inputs and digital I/O.   The analogue pins can be swapped and the digital pins can be swapped at will (with commensurate changes in the firmware).  I have set the swap levels on the part to allow this.  I put short wires on each pin and named them and did likewise with the parts they connected to.  The parts on the board layout are connected correctly but the layout would be better if some pins were swapped.   So, on the schematic I swap some pins and the board layout correctly reflects the changes.   The problem is that the schematic is now a mess wire wires draped all over the microcontroller.  I tried using Bus/Net but the result is similar.

 

Is there a way of using pinswap without making a mess of the schematic?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 7/02/2016 3:07 a.m., James Thurgood wrote:

    I am working on a design using a microcontroller using analogue inputs

    and digital I/O.   The analogue pins can be swapped and the digital pins

    can be swapped at will (with commensurate changes in the firmware).  I

    have set the swap levels on the part to allow this.  I put short wires

    on each pin and named them and did likewise with the parts they

    connected to.  The parts on the board layout are connected correctly but

    the layout would be better if some pins were swapped.   So, on the

    schematic I swap some pins and the board layout correctly reflects the

    changes.   The problem is that the schematic is now a mess wire wires

    draped all over the microcontroller.  I tried using Bus/Net but the

    result is similar.

     

    Is there a way of using pinswap without making a mess of the schematic?

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/173714

     

     

     

    Hi James

     

    It is what it is and the use of stub nets from the pins is as good as

    you can do.

     

    When the pin swap occurs, the end of the net segments attached to the

    pins are moved. If the last run to the pin is long, it appears as if

    lot of the schematic has been defaced.

     

    In this case there is a technique you can employ that you may benefit from.

     

    Just before you do the pin swap, drop a junction on the net just out

    from each of the pins you will swap. That will make the segment

    connected to the pin only as long as that from the junction to the pin,

    like a stub. In that way only the nets in the area of the pins are

    affected and the clean up is easier to envisage.

     

    HTH

    Warren

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • alberthall
    0 alberthall over 10 years ago in reply to autodeskguest

    So the short answer is 'no' - it can't be done.

    But my thanks to Warren for a suggestion to help minimise the mess.

     

    Ah, well, onwards and upwards...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • alberthall
    0 alberthall over 10 years ago in reply to autodeskguest

    So the short answer is 'no' - it can't be done.

    But my thanks to Warren for a suggestion to help minimise the mess.

     

    Ah, well, onwards and upwards...