Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Use None and All Libraries Still Show Up
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 630 views
  • Users 0 members are here
Related

Use None and All Libraries Still Show Up

e14 Contributor
e14 Contributor over 10 years ago

I'm having a problem with Eagle 7.3.0. I've selected Use none for a large number of libraries, and confirmed that the dot next to them is gray instead of green. However, when I click to add a component, I get all of the libraries. The libraries I'm trying to exclude are ones that are installed by Eagle. I event removed the $EAGLEDIR\lbr entry from the Directories dialog (from the Libraries text box), and they still show up. I also exited and restarted Eagle and they still show up.

 

Has anyone else run into this? Is this a known bug in 7.3? I tried 7.5, but I get the same issue.

 

Thanks,

  -- John

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 7/02/2016 12:36 p.m., John Socha-Leialoha wrote:

    I'm having a problem with Eagle 7.3.0. I've selected Use none for a

    large number of libraries, and confirmed that the dot next to them is

    gray instead of green. However, when I click to add a component, I get

    all of the libraries. The libraries I'm trying to exclude are ones that

    are installed by Eagle. I event removed the $EAGLEDIR\lbr entry from the

    Directories dialog (from the Libraries text box), and they still show

    up. I also exited and restarted Eagle and they still show up.

     

    Has anyone else run into this? Is this a known bug in 7.3? I tried 7.5,

    but I get the same issue.

     

    Thanks,

       -- John

     

    Hi

     

    I suspect you are using projects.

    Each project folder will have a file name eagle.epf

    Inside that file are the USED libraries from when the project was last

    closed.

    After closing a project, even if you UN-USE all the libraries in the

    control panel, when you open the project later the epf file is read and

    the libraries it contains are set to USE. If you now look at the control

    panel, all those libraries will now have the green dot/USED.

     

    You should be able UN-USE them all and to go back to the schematic where

    they should not appear on an ADD.

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    On 7/02/2016 1:12 p.m., warrenbrayshaw wrote:

    On 7/02/2016 12:36 p.m., John Socha-Leialoha wrote:

    I'm having a problem with Eagle 7.3.0. I've selected Use none for a

    large number of libraries, and confirmed that the dot next to them is

    gray instead of green. However, when I click to add a component, I get

    all of the libraries. The libraries I'm trying to exclude are ones that

    are installed by Eagle. I event removed the $EAGLEDIR\lbr entry from the

    Directories dialog (from the Libraries text box), and they still show

    up. I also exited and restarted Eagle and they still show up.

     

    Has anyone else run into this? Is this a known bug in 7.3? I tried 7.5,

    but I get the same issue.

     

    Thanks,

       -- John

     

    Hi

     

    I suspect you are using projects.

    Each project folder will have a file name eagle.epf

    Inside that file are the USED libraries from when the project was last

    closed.

    After closing a project, even if you UN-USE all the libraries in the

    control panel, when you open the project later the epf file is read and

    the libraries it contains are set to USE. If you now look at the control

    panel, all those libraries will now have the green dot/USED.

     

    You should be able UN-USE them all and to go back to the schematic where

    they should not appear on an ADD.

     

    HTH

    Warren

     

     

     

    I should add a couple more comments

     

    The epf could be pointing to libraries of an earlier version,when you

    used the project in that earlier/other version. Hence you are turning

    off the current version libraries but the older version libraries are

    being presented with the ADD.

     

    Open the eagle.epf file with a text editor. You should be able to see if

    this is the case

     

    You can delete the eagle.epf file of the project and another will

    created later

     

    All the best

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    On 7/02/2016 1:12 p.m., warrenbrayshaw wrote:

    On 7/02/2016 12:36 p.m., John Socha-Leialoha wrote:

    I'm having a problem with Eagle 7.3.0. I've selected Use none for a

    large number of libraries, and confirmed that the dot next to them is

    gray instead of green. However, when I click to add a component, I get

    all of the libraries. The libraries I'm trying to exclude are ones that

    are installed by Eagle. I event removed the $EAGLEDIR\lbr entry from the

    Directories dialog (from the Libraries text box), and they still show

    up. I also exited and restarted Eagle and they still show up.

     

    Has anyone else run into this? Is this a known bug in 7.3? I tried 7.5,

    but I get the same issue.

     

    Thanks,

       -- John

     

    Hi

     

    I suspect you are using projects.

    Each project folder will have a file name eagle.epf

    Inside that file are the USED libraries from when the project was last

    closed.

    After closing a project, even if you UN-USE all the libraries in the

    control panel, when you open the project later the epf file is read and

    the libraries it contains are set to USE. If you now look at the control

    panel, all those libraries will now have the green dot/USED.

     

    You should be able UN-USE them all and to go back to the schematic where

    they should not appear on an ADD.

     

    HTH

    Warren

     

     

     

    I should add a couple more comments

     

    The epf could be pointing to libraries of an earlier version,when you

    used the project in that earlier/other version. Hence you are turning

    off the current version libraries but the older version libraries are

    being presented with the ADD.

     

    Open the eagle.epf file with a text editor. You should be able to see if

    this is the case

     

    You can delete the eagle.epf file of the project and another will

    created later

     

    All the best

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to autodeskguest

    Yes, I'm using projects. I didn't have an eagle.epf file for the project I had open. However, there were eagle.epf files in other projects that were visible in the Control Panel. So I deleted all of those eagle.epf files, restarted Eagle, and I'm seeing the same thing. It's very odd... I do have Eagle 6.6 installed on my machine, as well as 7.3.0. Should I try removing Eagle 6.6?

     

    Thanks,

       -- John