Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Turn off thermals on selected components
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Subscribers 189 subscribers
  • Views 3440 views
  • Users 0 members are here
Related

Turn off thermals on selected components

zainka
zainka over 10 years ago

Hi

 

I have a design with several press-fit connectors. For these to turn off thermals would be a benefit. However, for other components which are soldered, thermals are required.

Is it possible to turn off thermals for individual components but leave them on for others?.

 

Thanks in advance

Vidar

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    vidar vidnes schrieb:

     

    I have a design with several press-fit connectors. For these to turn off

    thermals would be a benefit. However, for other components which are

    soldered, thermals are required.

    Is it possible to turn off thermals for individual components but leave

    them on for others?.

     

    In such cases, I simply draw multiple (overlapping) polygons with

    different "thermal" properties.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zainka
    0 zainka over 10 years ago in reply to autodeskguest

    Yes, that is an option, but I would prefer something that did not involve tweaking or workarounds.
    I have 5 pressfit connectors with 916 pin in total on a board with 14 layers. Many polygons in other words.

     

    I will suggest (in suggestion group) adding an thermal option / checkbox to component info-window, but i fear that will require a major code rewrite.

     

    Thanks

    Vidar (Z)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zainka
    0 zainka over 10 years ago in reply to autodeskguest

    Yes, that is an option, but I would prefer something that did not involve tweaking or workarounds.
    I have 5 pressfit connectors with 916 pin in total on a board with 14 layers. Many polygons in other words.

     

    I will suggest (in suggestion group) adding an thermal option / checkbox to component info-window, but i fear that will require a major code rewrite.

     

    Thanks

    Vidar (Z)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • zainka
    0 zainka over 10 years ago in reply to rachaelp

    Avoiding having several packages is all about effectiveness. To avoid having to update two packages in case of changes, and to limit the size of the library, and also having the ability to turn thermals individual on and off pr component, or pr. group, is nothing but a benefit. Adding to many polygons also slows down rendering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to autodeskguest

    Morten Leikvoll wrote on Thu, 14 April 2016 14:43

    Although I don't find this request relevant for pressfit, I have

    another use case for it. For capacitors (especially low ESR), you may

    want to avoid thermals by instance, not globally, but a polygon fill can

    also control this. A polygon with thermals=off will fill a smd/pad with

    thermals=on.

     

     

    Yep agreed, anywhere you care a lot about ESR/ESL or have particularly high current requirements, then this might be useful. You can do it with a polygon as you said or by package variants but this might be excessive to have additional packages defined for with thermals and without thermals on lots of generic parts, so having an easy checkbox to override the default on a per component basis might be useful.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to rachaelp

    Am 14.04.2016 um 15:40 schrieb rachaelp:

    vidar vidnes wrote:

     

    But I still wish for the option, as Rachel also suggested, to have the

    checkbox in the component properties in board layout.

    This because sometimes one wants to allow for the press-fit to be

    soldered. Then thermals should be there. I use the TE Tinman

    connectors, these have the option to be soldered aswell as to be

    "press-fitted"...  Having the checkbox avoids the need for two lib

    parts for same component.

    You could have two versions of the package, one with and one without

    thermals in your library for the same part. Then the different versions

    would be accesses by right clicking on a part and selecting "Package"

    from the context menu and selecting the alternative.

     

     

     

    Yes, that's the way you should do it.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to zainka

    On 14.04.2016 15:30, vidar vidnes wrote:

    Richard Hammerl wrote:

    there is an "Thermals" option for PADs and SMDs. This can be defined

    already in the library.

     

    @Vidar: You could change the pads' properties and do a library

    update in the drawing.

    Hmm, thats a good one. Already implemented, I like that and I will redo

    the library part.

    But I still wish for the option, as Rachel also suggested, to have the

    checkbox in the component properties in board layout.

    This because sometimes one wants to allow for the press-fit to be

    soldered. Then thermals should be there. I use the TE Tinman

    connectors, these have the option to be soldered aswell as to be

    "press-fitted"...  Having the checkbox avoids the need for two lib parts

    for same component.

     

    Problem would be to solve this if only some of the pins in the lib part

    has their thermals set to off in the library.

     

    (Maybe use a dropdown selection box instead where one have the options

    "As in library", "All off", "All on" and even "All off for pwr/sup pins"

    "All on for pwr/sup pins")

     

    Although I don't find this request relevant for pressfit, I have another

    use case for it. For capacitors (especially low ESR), you may want to

    avoid thermals by instance, not globally, but a polygon fill can also

    control this. A polygon with thermals=off will fill a smd/pad with

    thermals=on.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to zainka

    vidar vidnes wrote:

     

    But I still wish for the option, as Rachel also suggested, to have the checkbox in the component properties in board layout.

    This because sometimes one wants to allow for the press-fit to be soldered. Then thermals should be there. I use the TE Tinman

    connectors, these have the option to be soldered aswell as to be "press-fitted"...  Having the checkbox avoids the need for two lib parts for same component.

    You could have two versions of the package, one with and one without thermals in your library for the same part. Then the different versions would be accesses by right clicking on a part and selecting "Package" from the context menu and selecting the alternative.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zainka
    0 zainka over 10 years ago in reply to autodeskguest

    Richard Hammerl wrote:

    there is an "Thermals" option for PADs and SMDs. This can be defined

    already in the library.

     

    @Vidar: You could change the pads' properties and do a library

    update in the drawing.

    Hmm, thats a good one. Already implemented, I like that and I will redo the library part.

    But I still wish for the option, as Rachel also suggested, to have the checkbox in the component properties in board layout.

    This because sometimes one wants to allow for the press-fit to be soldered. Then thermals should be there. I use the TE Tinman

    connectors, these have the option to be soldered aswell as to be "press-fitted"...  Having the checkbox avoids the need for two lib parts for same component.

     

    Problem would be to solve this if only some of the pins in the lib part has their thermals set to off in the library.

     

    (Maybe use a dropdown selection box instead where one have the options

    "As in library", "All off", "All on" and even "All off for pwr/sup pins" "All on for pwr/sup pins")

     

     

    Vidar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to rachaelp

    Am 14.04.2016 um 13:22 schrieb rachaelp:

    Hi Vidar,

     

    A thermal option checkbox for each component is probably a reasonable

    suggestion. In addition to this I was thinking possibly it could also be

    something that is specified as part of the library part? After all, that

    press fit connector will want to not have thermals wherever it is used,

    so that info should really be stored with the part in the library I

    would think.

     

    Hi Rachel,

     

    there is an "Thermals" option for PADs and SMDs. This can be defined

    already in the library.

     

    @Vidar: You could change the pads' properties and do a library

    update in the drawing.

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to rachaelp

    rachaelp wrote:

     

    A thermal option checkbox for each component is probably a reasonable suggestion. In addition to this I was thinking possibly it could also be something that is specified as part of the library part? After all, that press fit connector will want to not have thermals wherever it is used, so that info should really be stored with the part in the library I would think.

    What I meant to say is you CAN specify this in the library as a specific through hole part as correctly mentioned by the subsequent poster as it's just a property of the pads in the package editor. It may still be useful to be able to turn this on and off at in the component properties dialog on a per component basis though as per your suggestion but not essential as it can be correctly specified in the part library.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to zainka

    Hi Vidar,

     

    A thermal option checkbox for each component is probably a reasonable suggestion. In addition to this I was thinking possibly it could also be something that is specified as part of the library part? After all, that press fit connector will want to not have thermals wherever it is used, so that info should really be stored with the part in the library I would think.

     

    Best Regards,

     

    Rachael