Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) multiple power sources on a single scheme
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 1167 views
  • Users 0 members are here
Related

multiple power sources on a single scheme

@xi@g@me
@xi@g@me over 10 years ago

Hi all ! I'm new to eagle, and am trying to create a scheme for a circuit which have different power sources.

The goal of this circuit is to emulate peripherals with a teensy board, and for this I need to do logic level translation. The chips that'll do the translations are bound to be powered from the machine the emulated peripheral is bound to be connected onto (not sure this is correct english, TBH).

 

On my first try, I get 4 peripherals to emulate on a single board, and so I got 5 different power sources (counting the teensy board)

I created different nets for each power source circuit, in order to have them correctly separated, and by avoiding the usage of the "Vcc" component.

 

However, when I try to do automatic routing on the generated board, all chips got their "Vcc" pins connected togother...

 

Is there a way for me to avoid that ?

 

Here is the scheme, exported as an image (didn't find a way to attach zip or sch files here)

Thanks in advance for your help image

 

image

  • Sign in to reply
  • Cancel
  • @xi@g@me
    0 @xi@g@me over 10 years ago in reply to autodeskguest

    CadSoft Guest a écrit:

     

    Check if your gnd/VCC pins are really connected to the wires in the

    schematic and not just accidentially ending there. The ERC will warn

    about this, but you can easily check by moving the devices with VCC

    around to see if the wire follows. If not, you need to drop it down

    again, and it will connect.

    There are some "visual issues" in eagle you need to be aware of. I think

    most of them happen if you copy and paste, move or bend wires.

     

    You can indeed override implicit power pins (pins defined with

    direction=pwr) like you have done. There will be a warning in the ERC

    about this, but it's ok to ignore. My ERC lists are usually flooded by

    these warnings.

     

    I just checked that, and they are all connected to their respective nets.

    However, I noticed that the Teensy had several GND and Vcc pins. I connected all of them to their respective nets, and now it works ! image

    Thanks all for your help image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • @xi@g@me
    0 @xi@g@me over 10 years ago in reply to autodeskguest

    CadSoft Guest a écrit:

     

    You appear to have connected "off-sheet labels" to the VCC pins. I'm not

    sure how exactly those work, since they're a new feature I haven't

    needed, but you may need to create a set of "VCCx" power symbols

    instead. At the very least, you need to make sure you've actually

    renamed the net connecting the pin to the label.

     

    What do you mean by "off-sheet labels" ? I can't control the labels directly, the name they display are the names of the nets connected to them. So yes, the nets are actually named correctly.

    Is there a link to a tutorial where I could create my own VCCx power supply symbols ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 19.04.2016 21:25, Grégoire MATHIEU wrote:

    Hi all ! I'm new to eagle, and am trying to create a scheme for a

    circuit which have different power sources.

    The goal of this circuit is to emulate peripherals with a teensy board,

    and for this I need to do logic level translation. The chips that'll do

    the translations are bound to be powered from the machine the emulated

    peripheral is bound to be connected onto (not sure this is correct

    english, TBH).

     

    On my first try, I get 4 peripherals to emulate on a single board, and

    so I got 5 different power sources (counting the teensy board)

    I created different nets for each power source circuit, in order to have

    them correctly separated, and by avoiding the usage of the "Vcc"

    component.

     

    However, when I try to do automatic routing on the generated board, all

    chips got their "Vcc" pins connected togother...

     

    Is there a way for me to avoid that ?

     

    Here is the scheme, exported as an image (didn't find a way to attach

    zip or sch files here)

    Thanks in advance for your help image

     

     

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/195087

     

     

    Check if your gnd/VCC pins are really connected to the wires in the

    schematic and not just accidentially ending there. The ERC will warn

    about this, but you can easily check by moving the devices with VCC

    around to see if the wire follows. If not, you need to drop it down

    again, and it will connect.

    There are some "visual issues" in eagle you need to be aware of. I think

    most of them happen if you copy and paste, move or bend wires.

     

    You can indeed override implicit power pins (pins defined with

    direction=pwr) like you have done. There will be a warning in the ERC

    about this, but it's ok to ignore. My ERC lists are usually flooded by

    these warnings.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 19/04/16 20:25, Grégoire MATHIEU wrote:

    However, when I try to do automatic routing on the generated board, all

    chips got their "Vcc" pins connected togother...

     

    Is there a way for me to avoid that ?

     

    You appear to have connected "off-sheet labels" to the VCC pins. I'm not

    sure how exactly those work, since they're a new feature I haven't

    needed, but you may need to create a set of "VCCx" power symbols

    instead. At the very least, you need to make sure you've actually

    renamed the net connecting the pin to the label.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    Why not eliminate +3.3 Volts since this is not common source. You can create a circuit to change +5.0 volts down to 3.3 volts with a DC DC buck converter IC.

    Clem