Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Problem with creating library
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 189 subscribers
  • Views 544 views
  • Users 0 members are here
Related

Problem with creating library

e14 Contributor
e14 Contributor over 10 years ago

Hi all,

 

I have a peculiar problem while creating a library part. The package was created. Then the symbol a 16 pin device. However when linking the device it pops up with package doesn't have enough pads to cover the number of pins created. Upon further investigation, I found that every pin is linked twice. By that I mean when I just have 1 pin in the Symbol (as opposed to 16), save then go to Device and click Connect, the name of pin 1 appears twice as follows: G$1.P$1 and G$2.P$1.

So if I had the full 16, that would mean 32 and obviously 16 pads cannot cover the pins.

 

So how do I get rid of the double pin linkage?

 

Eagle version 6.5 Professional.

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    0 rachaelp over 10 years ago

    That sounds like you have two copies of the symbol placed in the device editor. Is it possible you somehow added two and they are sat right on top of each other so you can't tell there is more than one?

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • rachaelp
    0 rachaelp over 10 years ago

    That sounds like you have two copies of the symbol placed in the device editor. Is it possible you somehow added two and they are sat right on top of each other so you can't tell there is more than one?

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rachaelp

    Correct, when I clicked on the create overall package, I somehow placed 2 copies. Very weird. Thanks for the reply.