Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Issue connecting wire
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 189 subscribers
  • Views 876 views
  • Users 0 members are here
Related

Issue connecting wire

e14 Contributor
e14 Contributor over 10 years ago

Hello .I am undergoing with below issue. I tried to resolve by checking some online tutorials but I cant find out the solution.

Issue:

 

I cant find LT3751 device in Eagle library and I created my own. But I cannot connect the wire from an component to my device. I am using Eagle 7.5 Version.

 

please find attachment.

 

1. Wire connection

2.Grid config

3.Library file

 

 

Thanks for your support.

Attachments:
lbr and Screenshot.zip
  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    0 rachaelp over 10 years ago

    Hi,

     

    I've just had a quick look at your library and the problem is because you haven't drawn the symbol in your library on a 0.1" grid. Pretty much all the pins are off grid which is why it won't connect. You need to change your grid in your library symbol to 0.1" and move all the pins back onto the grid.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rachaelp
    0 rachaelp over 10 years ago

    Hi,

     

    I've just had a quick look at your library and the problem is because you haven't drawn the symbol in your library on a 0.1" grid. Pretty much all the pins are off grid which is why it won't connect. You need to change your grid in your library symbol to 0.1" and move all the pins back onto the grid.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rachaelp

    Thank you for your support Rachaelp. I did as said and my problem was solved.

    I have small clarification.

     

    I need a ceramic capacitor

     

    Length: 6 mm
    Width: 5.5 mm
    Height: 3.5 mm
    Lead Diameter: 0.5 mm
    ff

     

     

    From eagle library I found :

    CAPACITOR naming: grid - package width

    Package: C5B3.5
    MKS2, 7.5 x 4 mm, grid 5.08 mm

     

    My doubt is that :

     

    1.  7.5mm is length? 4mm is width and 5.08 is hole to hole spacing  (distance between two holes).?

     

    2. Lead diameter is 0.5mm that is what i needed. so the hole size in layout should be same 0.5mm. where can I verify the hole size If I take a capacitor from the library.

     

    3. Is the possible to increase the hole size and distance between the 2  holes in the layout.

     

     

    Thank you very much in advance. This could be my last issue.

     

     

    have a great day!