Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How do I create mounting hole with vias
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Answers 2 answers
  • Subscribers 188 subscribers
  • Views 4886 views
  • Users 0 members are here
  • mounting hole with vias
Related

How do I create mounting hole with vias

markusbass
markusbass over 10 years ago

I'm looking for a way to create mounting hole with 6 vias (as a library component) for M3 screw. I was able to create such a package but when I use it on a board and run DRC, I get "Overlap" errors. The vias are defined as small pads since vias are not available in library designer. Is there a way to get rid of the errors? I remember that I was able to define such a component in KiCAD and I' surprised that in Eagle it is that difficult.

Here: pcb design - Mounting hole on a PCB - Electrical Engineering Stack Exchange  is an example of such a mounting hole (the right most on the photo).

 

Mark

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 02.06.2016 19:22, Marek Kepinski wrote:

    I'm looking for a way to create mounting hole with 6 vias (as a library component) for M3 screw. I was able to create such a package but when I use it on a board and run DRC, I get "Overlap" errors. The vias are defined as small pads since vias are not available in library designer. Is there a way to get rid of the errors? I remember that I was able to define such a component in KiCAD and I' surprised that in Eagle it is that difficult.

    Here: pcb design - Mounting hole on a PCB - Electrical Engineering Stack Exchange (http://electronics.stackexchange.com/questions/137394/mounting-hole-on-a-pcb)  is an example of such a mounting hole (the right most on the photo).

     

    First, at the rightmost picture on the link you send, the vias are not

    needed, as the hole is already plated, but I think it can be done with a

    large pad + smaller pads overlapping all in the package. And all those

    pads need to be appended to a single symbol pin.

     

    If you prefer the non plated (middle pic), your package needs vias

    surrounded with a polygon, all appended to one pin, and the masks

    manually made ofcourse.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • markusbass
    0 markusbass over 10 years ago in reply to autodeskguest

    Thanks for the answer but I need a little bit more information on the "append" action. I tried it but the "Overlap" error didn't disappear. I also get some other strange problems: I add the package to the board (it is connected to GND on the schematic). I surround the package with a polygon, rename it to GND and fill with ratsnest. At this moment the two small pads ("vias") are connected with a track, the polygon disappears. My target is to get rid of the "Overlap" error and to be able to connect it to GND, or leave it unconnected (with filled polygons around the package). Any ideas?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • markusbass
    0 markusbass over 10 years ago in reply to markusbass

    I have some progress. The problems that I had with polygon were a result of the way I tested the package. There were no other tracks on the board and no other components inside the polygon. After correcting this the solution almost works. It looks like this:image

    The "Overlap" error is not reported now. But the pad is not connected to the ground despite the fact that the polygon is "GND" , the mounting holes are connected to GND on the schematic and the package has "Thermals" option checked. How can I correct this problem?

    Also two vias are connected with track but this will be removed during drilling of the board. Why this track is displayed?

    The current solution uses "append" feature (as suggested), the pads are marked as disconnected (with little green icon) and "@x" in the names of the small pads (but I'm not sure whether this is important).

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • markusbass
    0 markusbass over 10 years ago in reply to autodeskguest

    Yes, they had "Thermals" flag checked. Also the "Stop" flag was checked. I think both are not needed.

    Thank you very much for your help.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to markusbass

    On 05.06.2016 18:52, markusbass wrote:

    Thank you very much. yes, this was the problem. Adding a stub net to that pin solved the problem. I'd like to mark this answer as "Correct Answer" but the answer is spread between various posts.

    I have just last question:

    It seems that there are still some differences between my a Warren's library. When I move the grounded pads away, one can see that the thermal tracks generated with my library are different width, while tracks from Warren's library are perfect.

    What can cause this difference?

     

    Wild guess; the small pads should have thermal off, while the big one

    should have thermal on?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • markusbass
    0 markusbass over 10 years ago in reply to autodeskguest

    Thank you very much. yes, this was the problem. Adding a stub net to that pin solved the problem. I'd like to mark this answer as "Correct Answer" but the answer is spread between various posts.

    I have just last question:

    It seems that there are still some differences between my a Warren's library. When I move the grounded pads away, one can see that the thermal tracks generated with my library are different width, while tracks from Warren's library are perfect.

    image

    What can cause this difference?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • markusbass
    0 markusbass over 10 years ago in reply to autodeskguest

    Thank you very much. yes, this was the problem. Adding a stub net to that pin solved the problem. I'd like to mark this answer as "Correct Answer" but the answer is spread between various posts.

    I have just last question:

    It seems that there are still some differences between my a Warren's library. When I move the grounded pads away, one can see that the thermal tracks generated with my library are different width, while tracks from Warren's library are perfect.

    image

    What can cause this difference?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • markusbass
    0 markusbass over 10 years ago in reply to autodeskguest

    Yes, they had "Thermals" flag checked. Also the "Stop" flag was checked. I think both are not needed.

    Thank you very much for your help.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to markusbass

    On 05.06.2016 18:52, markusbass wrote:

    Thank you very much. yes, this was the problem. Adding a stub net to that pin solved the problem. I'd like to mark this answer as "Correct Answer" but the answer is spread between various posts.

    I have just last question:

    It seems that there are still some differences between my a Warren's library. When I move the grounded pads away, one can see that the thermal tracks generated with my library are different width, while tracks from Warren's library are perfect.

    What can cause this difference?

     

    Wild guess; the small pads should have thermal off, while the big one

    should have thermal on?