Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) rename multiple vias at the same time
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 2941 views
  • Users 0 members are here
  • name
  • vias
Related

rename multiple vias at the same time

e14 Contributor
e14 Contributor over 10 years ago

Hello,

I am placing multiple vias next to each other in order to electrically connect two polygons (top and bottom) of the same net. When placing the vias, each one has a unique name. Hence, the vias are not connected to the polygons. So I am using the name-tool now to rename each via one by one. The group-function does not work.

Is there a faster way of renaming the vias so all of them are within the same net as the polygons at once? Maybe directly when placing them?

 

Thank you!

Lars

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 07/07/2016 03:52 AM, Lars Middelstaedt wrote:

    Hello,

    I am placing multiple vias next to each other in order to electrically connect two polygons (top and bottom) of the same net. When placing the vias, each one has a unique name. Hence, the vias are not connected to the polygons. So I am using the name-tool now to rename each via one by one. The group-function does not work.

    Is there a faster way of renaming the vias so all of them are within the same net as the polygons at once? Maybe directly when placing them?

     

    Thank you!

    Lars

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/200935

     

     

    Place the first via with the same net name as the polygon then copy the via to other places. The copies will retain the

    net name as long as the via doesn't use an Eagle generated name. You can then copy the copies as you would the first via.

     

    Eric

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to autodeskguest

    Thanks for that easy solution image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to autodeskguest

    Thanks for that easy solution image