Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 7.6.0 constantly crashing - what to do?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 39 replies
  • Answers 4 answers
  • Subscribers 193 subscribers
  • Views 7287 views
  • Users 0 members are here
  • 7.6.0
  • crash
  • crashing
  • 7.6
  • mac
Related

Eagle 7.6.0 constantly crashing - what to do?

tomstorey
tomstorey over 10 years ago

Hi everyone. I'm at a loss as to how to handle this situation.

 

I'd been using Eagle freeware for about a month flawlessly, but over the last two weeks or so I can barely do more than 5 minutes of work without it crashing and burning (well, not exactly burning.)

 

Simple things like zooming in and out of a schematic, scrolling in a schematic, or even clicking on a button on a toolbar will cause it to crash. So far I've spent most of my time in the schematic editor, so I'm not 100% sure if it also happens in the PCB editor.

 

I'm running it on a Mac (10.10), and I was also seeing the same problem with 7.5.0. Rather conveniently 7.6.0 came out not long after I started seeing the crashes with 7.5.0, so I upgraded hoping that might help, but alas, 7.6.0 had the exact same problem.

 

I tried restarting, I completely deleted the Eagle application folder and re-installed, but neither of those did anything to help. Can anyone suggest anything else?

 

The first tell-tale signs its about to happen are when I start to see graphical glitches, like that in the attached screenshot. Then, a couple of clicks later, boom - crash. I'm at the stage where I'm constantly saving my work in fear of losing it.

 

I'm really really liking Eagle, and Ive been considering purcashing a license, but if its going to behave like this, I dunno ....... image

 

Many thanks.

Tom

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi,

     

    I have exactly the same problem, when I use multiple monitors. I have a MacBook Pro Retina connected via HDMI to a standard HD monitor, and if the external monitor is connected EAGLE will crash after a few minutes, usually when zooming in or out with the mousewheel. Crashes are often preceded by the graphic corruption described by Tom.

     

    Maybe it's related to having a hi-dpi screen and a standard DPI screen in use at the same time?

     

    The crashes still occur even if the external screen is 'mirroring' the laptop screen.

     

    It's quite annoying having to unplug the big screen just to use EAGLE... but so far EAGLE still seems to be stable when using just the laptop screen.

     

    Thx, Kieran.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi,

     

    I have exactly the same problem, when I use multiple monitors. I have a MacBook Pro Retina connected via HDMI to a standard HD monitor, and if the external monitor is connected EAGLE will crash after a few minutes, usually when zooming in or out with the mousewheel. Crashes are often preceded by the graphic corruption described by Tom.

     

    Maybe it's related to having a hi-dpi screen and a standard DPI screen in use at the same time?

     

    The crashes still occur even if the external screen is 'mirroring' the laptop screen.

     

    It's quite annoying having to unplug the big screen just to use EAGLE... but so far EAGLE still seems to be stable when using just the laptop screen.

     

    Thx, Kieran.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • tomstorey
    0 tomstorey over 10 years ago in reply to e14 Contributor

    Thats interesting, because I also use an external screen on a MacBook Pro Retina.