Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 7.6.0 constantly crashing - what to do?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 39 replies
  • Answers 4 answers
  • Subscribers 193 subscribers
  • Views 7258 views
  • Users 0 members are here
  • 7.6.0
  • crash
  • crashing
  • 7.6
  • mac
Related

Eagle 7.6.0 constantly crashing - what to do?

tomstorey
tomstorey over 10 years ago

Hi everyone. I'm at a loss as to how to handle this situation.

 

I'd been using Eagle freeware for about a month flawlessly, but over the last two weeks or so I can barely do more than 5 minutes of work without it crashing and burning (well, not exactly burning.)

 

Simple things like zooming in and out of a schematic, scrolling in a schematic, or even clicking on a button on a toolbar will cause it to crash. So far I've spent most of my time in the schematic editor, so I'm not 100% sure if it also happens in the PCB editor.

 

I'm running it on a Mac (10.10), and I was also seeing the same problem with 7.5.0. Rather conveniently 7.6.0 came out not long after I started seeing the crashes with 7.5.0, so I upgraded hoping that might help, but alas, 7.6.0 had the exact same problem.

 

I tried restarting, I completely deleted the Eagle application folder and re-installed, but neither of those did anything to help. Can anyone suggest anything else?

 

The first tell-tale signs its about to happen are when I start to see graphical glitches, like that in the attached screenshot. Then, a couple of clicks later, boom - crash. I'm at the stage where I'm constantly saving my work in fear of losing it.

 

I'm really really liking Eagle, and Ive been considering purcashing a license, but if its going to behave like this, I dunno ....... image

 

Many thanks.

Tom

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • mrmarple
    0 mrmarple over 10 years ago

    Eagle 7.6.0 running on a Hac (yes Hac) with OSX 10.10.5 Yosemite and two

    monitors is stable here, no unexpected crashes. I can crash it, I avoid the

    one situation that I know is a problem.

     

    Starting eagle from the desktop by double clicking on a board icon, it

    might be a downloaded board, or a board not in a project. The board

    opens but a mouse wheel zoom kills Eagle, resize the window before zooming

    and all is fine.

     

    If do anything unusual in Eagle I quit and restart.

     

    I turned file locking off early on, what is the intent of this feature?

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mrmarple
    0 mrmarple over 10 years ago

    Eagle 7.6.0 running on a Hac (yes Hac) with OSX 10.10.5 Yosemite and two

    monitors is stable here, no unexpected crashes. I can crash it, I avoid the

    one situation that I know is a problem.

     

    Starting eagle from the desktop by double clicking on a board icon, it

    might be a downloaded board, or a board not in a project. The board

    opens but a mouse wheel zoom kills Eagle, resize the window before zooming

    and all is fine.

     

    If do anything unusual in Eagle I quit and restart.

     

    I turned file locking off early on, what is the intent of this feature?

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • vintagesynthlab
    0 vintagesynthlab over 10 years ago in reply to mrmarple

    Ken-

    Thank you!  See my comment below (the resizing technique seems to work for me as a temp solution).

     

    Regards,

    Eric