Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 7.6.0 constantly crashing - what to do?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 39 replies
  • Answers 4 answers
  • Subscribers 193 subscribers
  • Views 7290 views
  • Users 0 members are here
  • 7.6.0
  • crash
  • crashing
  • 7.6
  • mac
Related

Eagle 7.6.0 constantly crashing - what to do?

tomstorey
tomstorey over 10 years ago

Hi everyone. I'm at a loss as to how to handle this situation.

 

I'd been using Eagle freeware for about a month flawlessly, but over the last two weeks or so I can barely do more than 5 minutes of work without it crashing and burning (well, not exactly burning.)

 

Simple things like zooming in and out of a schematic, scrolling in a schematic, or even clicking on a button on a toolbar will cause it to crash. So far I've spent most of my time in the schematic editor, so I'm not 100% sure if it also happens in the PCB editor.

 

I'm running it on a Mac (10.10), and I was also seeing the same problem with 7.5.0. Rather conveniently 7.6.0 came out not long after I started seeing the crashes with 7.5.0, so I upgraded hoping that might help, but alas, 7.6.0 had the exact same problem.

 

I tried restarting, I completely deleted the Eagle application folder and re-installed, but neither of those did anything to help. Can anyone suggest anything else?

 

The first tell-tale signs its about to happen are when I start to see graphical glitches, like that in the attached screenshot. Then, a couple of clicks later, boom - crash. I'm at the stage where I'm constantly saving my work in fear of losing it.

 

I'm really really liking Eagle, and Ive been considering purcashing a license, but if its going to behave like this, I dunno ....... image

 

Many thanks.

Tom

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    This has happened to many others when you run out of memory. Try to close other windows and avoid operations like Ratnest over many connections.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tomstorey
    0 tomstorey over 10 years ago in reply to clem57

    Thanks Clem.

     

    Shame that it is unable to handle that a bit more gracefully. No other application that I'm running has such brutal behaviour.

     

    I do have a few tabs open in Chrome, which is notoriously memory hungry. I'll give it another reboot and try before re-opening Chrome.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tomstorey
    0 tomstorey over 10 years ago in reply to clem57

    Thanks Clem.

     

    Shame that it is unable to handle that a bit more gracefully. No other application that I'm running has such brutal behaviour.

     

    I do have a few tabs open in Chrome, which is notoriously memory hungry. I'll give it another reboot and try before re-opening Chrome.