Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 7.6.0 constantly crashing - what to do?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 39 replies
  • Answers 4 answers
  • Subscribers 193 subscribers
  • Views 7290 views
  • Users 0 members are here
  • 7.6.0
  • crash
  • crashing
  • 7.6
  • mac
Related

Eagle 7.6.0 constantly crashing - what to do?

tomstorey
tomstorey over 10 years ago

Hi everyone. I'm at a loss as to how to handle this situation.

 

I'd been using Eagle freeware for about a month flawlessly, but over the last two weeks or so I can barely do more than 5 minutes of work without it crashing and burning (well, not exactly burning.)

 

Simple things like zooming in and out of a schematic, scrolling in a schematic, or even clicking on a button on a toolbar will cause it to crash. So far I've spent most of my time in the schematic editor, so I'm not 100% sure if it also happens in the PCB editor.

 

I'm running it on a Mac (10.10), and I was also seeing the same problem with 7.5.0. Rather conveniently 7.6.0 came out not long after I started seeing the crashes with 7.5.0, so I upgraded hoping that might help, but alas, 7.6.0 had the exact same problem.

 

I tried restarting, I completely deleted the Eagle application folder and re-installed, but neither of those did anything to help. Can anyone suggest anything else?

 

The first tell-tale signs its about to happen are when I start to see graphical glitches, like that in the attached screenshot. Then, a couple of clicks later, boom - crash. I'm at the stage where I'm constantly saving my work in fear of losing it.

 

I'm really really liking Eagle, and Ive been considering purcashing a license, but if its going to behave like this, I dunno ....... image

 

Many thanks.

Tom

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • doubletop
    0 doubletop over 10 years ago

    Me too

     

    A new Dell Inspiron 13 7000, I7 CPU and 8Gb memory. One week old with only Windows 10, Office Home, Firefox, Thunderbird Eagle 7.6.0 and MPLAB X 3.3.5. That’s it.

     

    Eagle in free mode and a simple circuit 2 x  INA126 and a PIC 16F1847 with a handful of discrete components and connectors. Inconsistencies get reported when I select Autorouter and after checking and fixing all inconsistences in ERC I still get the report. If I ignore the inconsistencies the pop up keeps re-appearing and then the system crashes. I've been doing a regular save all" and still the inconsistencies start.

     

    So far I've made progress by deleting the .brd file and the re making it from the schematic and laying it out again. After a few modifications it starts the inconsistencies thing again and then crashes

     

     

    .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • doubletop
    0 doubletop over 10 years ago

    Me too

     

    A new Dell Inspiron 13 7000, I7 CPU and 8Gb memory. One week old with only Windows 10, Office Home, Firefox, Thunderbird Eagle 7.6.0 and MPLAB X 3.3.5. That’s it.

     

    Eagle in free mode and a simple circuit 2 x  INA126 and a PIC 16F1847 with a handful of discrete components and connectors. Inconsistencies get reported when I select Autorouter and after checking and fixing all inconsistences in ERC I still get the report. If I ignore the inconsistencies the pop up keeps re-appearing and then the system crashes. I've been doing a regular save all" and still the inconsistencies start.

     

    So far I've made progress by deleting the .brd file and the re making it from the schematic and laying it out again. After a few modifications it starts the inconsistencies thing again and then crashes

     

     

    .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • doubletop
    0 doubletop over 10 years ago in reply to doubletop

    I just finished typing the last post and then tried this.

     

    After the crash there are two .lck lock files. Delete them and then restart the console. Open the schematic and save as a different file name. The .brd file opened as well and was also renamed. The Autorouter then worked properly.

     

    Beats me but I managed to move forwards