Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 7.6.0 constantly crashing - what to do?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 39 replies
  • Answers 4 answers
  • Subscribers 193 subscribers
  • Views 7284 views
  • Users 0 members are here
  • 7.6.0
  • crash
  • crashing
  • 7.6
  • mac
Related

Eagle 7.6.0 constantly crashing - what to do?

tomstorey
tomstorey over 10 years ago

Hi everyone. I'm at a loss as to how to handle this situation.

 

I'd been using Eagle freeware for about a month flawlessly, but over the last two weeks or so I can barely do more than 5 minutes of work without it crashing and burning (well, not exactly burning.)

 

Simple things like zooming in and out of a schematic, scrolling in a schematic, or even clicking on a button on a toolbar will cause it to crash. So far I've spent most of my time in the schematic editor, so I'm not 100% sure if it also happens in the PCB editor.

 

I'm running it on a Mac (10.10), and I was also seeing the same problem with 7.5.0. Rather conveniently 7.6.0 came out not long after I started seeing the crashes with 7.5.0, so I upgraded hoping that might help, but alas, 7.6.0 had the exact same problem.

 

I tried restarting, I completely deleted the Eagle application folder and re-installed, but neither of those did anything to help. Can anyone suggest anything else?

 

The first tell-tale signs its about to happen are when I start to see graphical glitches, like that in the attached screenshot. Then, a couple of clicks later, boom - crash. I'm at the stage where I'm constantly saving my work in fear of losing it.

 

I'm really really liking Eagle, and Ive been considering purcashing a license, but if its going to behave like this, I dunno ....... image

 

Many thanks.

Tom

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • tomstorey
    0 tomstorey over 10 years ago

    I really dont want to jinx this, but for the last 2 days Eagle has been running flawlessly again for me.

     

    Although its nice, its still somewhat of a worry - what was causing the crashes before, and will they come back, and if they do how long before they go away again? image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • doubletop
    0 doubletop over 10 years ago in reply to tomstorey

    I saved the schematic as a new file and re-created the board. Did the ERC/DRC checks on both and fixed everything , no errors and announced that both drawings were consistent. Ran Autorouter and was told both were now inconsistent. back out of Autorouter checked again and both were consistent. back into Autorouter both inconsistent. The other thing was all the drop downs were greyed out. It was at this point I knew that selecting "do you want to run anyway" which will pop up a few times and if you keep saying yes Eagle will crash. However I then I noticed the check box, "do you want to continue with the previous run" I unselected it and the greyed out boxes were accessible again and the autorouter ran fine.

     

    I think that was probably it all along. I'll keep and eye out for it again. If the autorouter fails or is stopped for any reason uncheck that checkbox

     

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tomstorey
    0 tomstorey over 10 years ago in reply to doubletop

    If I think back, I renamed my schematic and deleted my board to start over again. This may have helped me with my crashes.....

    Why, I have no idea, seems crazy and odd. But it may have played a part. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tomstorey
    0 tomstorey over 10 years ago in reply to doubletop

    If I think back, I renamed my schematic and deleted my board to start over again. This may have helped me with my crashes.....

    Why, I have no idea, seems crazy and odd. But it may have played a part. image