Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Compact Address selection method
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 189 subscribers
  • Views 1380 views
  • Users 0 members are here
Related

Compact Address selection method

e14 Contributor
e14 Contributor over 10 years ago

Hi,

 

I have a couple of I2C devices which have address selection inputs A0,A1,A2. These can happily be connected to Ground = 0 or VDD = 1. I need both chips to be on the same address (they have different I2C base addresses).

 

All very simple stuff - I can connect the address lines of the two chips in parallel and use jumpers to select the address by connecting the pins to Ground or VDD like this:

 

image

 

Now, my question is this: What is the most compact way of achieving this?

 

I am very pressed for space, and two rows of standard 2.54mm-spaced jumper headers look simply enormous on a compact board.

 

One option is to use a Resistor Network to pull the lines up to VDD, and double row of jumpers (or DIP switches) to pull them individually to ground though that, if anything, takes up more space than a triple row of jumpers. Ditto an 8-way rotary address selector and a Resistor Network.

 

I could just terminate on pads, make sure there's no solder mask, and bridge the appropriate pads with blobs of solder, but then that's not very nice if I want to change the address in the future (which the user might though not often).

 

Anybody got a neat space-saving way of doing this?

 

Richard

  • Sign in to reply
  • Cancel
Parents
  • e14candies
    0 e14candies over 10 years ago

    If you are using I2C, could you use software controlled pins on your micro

    & a terminal to set them?  I don't have a pic of your system. Just store

    the settings in internal EEPROM or flash, if you have some avail.

     

    Here are some more of the 1.27mm shunts:

     

    http://www.isipkg.com/images/products/connectors/standard/Jumpers-shunts/Jumpers%201mm/92B-1.pdf

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14candies
    0 e14candies over 10 years ago

    If you are using I2C, could you use software controlled pins on your micro

    & a terminal to set them?  I don't have a pic of your system. Just store

    the settings in internal EEPROM or flash, if you have some avail.

     

    Here are some more of the 1.27mm shunts:

     

    http://www.isipkg.com/images/products/connectors/standard/Jumpers-shunts/Jumpers%201mm/92B-1.pdf

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14candies

    Norm: that'd be a very sensible idea, however this is Raspberry Pi peripheral and, believe it or not, I have a use for every one of the useable GPIO pins so I'd have to add a GPIO expander, which sort-of defeats the object!

     

    I think I'll go with the 1.27mm jumper idea.

     

    Richard