Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Wiring problem on Eagle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 4278 views
  • Users 0 members are here
  • eagle
  • wire to wire
  • symbol
Related

Wiring problem on Eagle

e14 Contributor
e14 Contributor over 10 years ago

Hello,

I got a problem because I can't wire to a component I created. First, I created a library for the component with Symbol, then Package and Device.

But when I am using this component on my schematic, I can't wire it. I used the same scale and grid for all the schematics and I updated libraries. But it is impossible to wire it.

If anyone has an idea to solve my problem ?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 7/22/2016 11:42 AM, djib ty wrote:

    Hello,

    I got a problem because I can't wire to a component I created. First, I created a library for the component with Symbol, then Package and Device.

    But when I am using this component on my schematic, I can't wire it. I used the same scale and grid for all the schematics and I updated libraries. But it is impossible to wire it.

    If anyone has an idea to solve my problem ?

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/202123

     

    Hi Djib,

     

    I hope you're doing well. Make sure that the part was made to a 0.1"

    grid. Also in order to see the connection points clearly turn on layer

    93 Pins in the schematic. You will now see lots of green circles one for

    each pin. The center of those circles is the connection point, all of

    your nets must start and end on the exact center of these circles(this

    is why it's important to stay on a 0.1" grid). If you don't see green

    circles on your part then that means you didn't use the PIN command and

    you need to go back to your library and create pins. One final thing to

    check make sure you are using the NET command to create your connections.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 7/22/2016 11:42 AM, djib ty wrote:

    Hello,

    I got a problem because I can't wire to a component I created. First, I created a library for the component with Symbol, then Package and Device.

    But when I am using this component on my schematic, I can't wire it. I used the same scale and grid for all the schematics and I updated libraries. But it is impossible to wire it.

    If anyone has an idea to solve my problem ?

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/202123

     

    Hi Djib,

     

    I hope you're doing well. Make sure that the part was made to a 0.1"

    grid. Also in order to see the connection points clearly turn on layer

    93 Pins in the schematic. You will now see lots of green circles one for

    each pin. The center of those circles is the connection point, all of

    your nets must start and end on the exact center of these circles(this

    is why it's important to stay on a 0.1" grid). If you don't see green

    circles on your part then that means you didn't use the PIN command and

    you need to go back to your library and create pins. One final thing to

    check make sure you are using the NET command to create your connections.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to autodeskguest

    Hello Jorge,

     

    I turned on layer 93 Pins on the schematic and I can see green circles for each pin of my component.

    Unfortunately, I still can't wire it because the nets don't start or end on the exact center of the circles.

    Meanwhile, I used 0.1 inch grid for Symbol, Package and Device. Then, I updated libraries but it's the same problems with nets which can't connect in the exact center of the circles.