Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Consistency errors
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 36 replies
  • Subscribers 189 subscribers
  • Views 3397 views
  • Users 0 members are here
Related

Consistency errors

maciv4
maciv4 over 10 years ago

I have 5 consistency errors, on sections of my board that I wired several days ago. One of the errors is on an airwire. Do I have to delete the entire net to find the offending trace. I also have missing airwires; parts with no airwires attached at one end. I also have airwires still in place after I have placed traces, that ratsnest won't clear. I assume that the consistency errors are preventing annotation between the schematic and the board. Can you help?

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    0 rachaelp over 10 years ago

    Hi Jim,

     

    Did you edit the schematic or board without the corresponding file open?

    This is a guaranteed way to create consistency errors. The missing air

    wires would probably be because the net was added in the schematic while

    back annotation wasn't working so the board knows nothing about the net.

     

    You've not really given enough information about what the errors actually

    are for us to be able to help, can you post up what the actual messages are

    saying?

     

    Basically what you'll need to do is back out any additions to the schematic

    that happened while not in sync and make sure any property changes are in

    sync across both the schematic and the board. Keep running ERC and working

    through the list of differences until you see all the errors are cleared.

    If you can supply more info then we can probably help more.

     

    Best Regards,

     

    Rachael

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rachaelp
    0 rachaelp over 10 years ago

    Hi Jim,

     

    Did you edit the schematic or board without the corresponding file open?

    This is a guaranteed way to create consistency errors. The missing air

    wires would probably be because the net was added in the schematic while

    back annotation wasn't working so the board knows nothing about the net.

     

    You've not really given enough information about what the errors actually

    are for us to be able to help, can you post up what the actual messages are

    saying?

     

    Basically what you'll need to do is back out any additions to the schematic

    that happened while not in sync and make sure any property changes are in

    sync across both the schematic and the board. Keep running ERC and working

    through the list of differences until you see all the errors are cleared.

    If you can supply more info then we can probably help more.

     

    Best Regards,

     

    Rachael

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • maciv4
    0 maciv4 over 10 years ago in reply to rachaelp

    The errors are as follows:

     

     

    Different connections on R48 pin 2 and pad 2 (-12V/$$1) 2

    Different connections on R84 pin 2 and pad 2 (-12V/$$1) 3

    Different connections on U15P pin V- and pad 4 (-12V/$$1) 2

    Different connections on U17P pin V- and pad 4 (-12V/$$1) 3

    Different connections on U20P pin V- and pad 4 (-12V/$$1) 3

     

    I always open the schematic first and then open the board from the schematic. I need one to finish wireing the other. There may be traces that I have added since this problem started, that I expect, but I have errors on traces I did last week. All of these errors are on traces that I did last week before any of these problems arose. I have opened, saved, and closed these files multiple times in between.

     

     

    How do I clear these errors? Do I have to retrace the -12V node? The entire board? I've already tried retracing the traces between the different parts. I have also tried deleteing, saving and replacing the parts.