Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Making parts from datasheet into eagle library
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 466 views
  • Users 0 members are here
Related

Making parts from datasheet into eagle library

e14 Contributor
e14 Contributor over 10 years ago

I have to use a specific type of capacitor in making a circuit board. I have not found any CAD designs for this capacitor. I use the dimensions from the datasheet, but it seems that the width of the line is making the parts larger. For example if I have to make a 3mm by 3mm square, and I use the polygon function, and use (0,0) (3,0) (3,3)(0,3). Then I change the grid to make the boxes 3mm boxes, the square will be larger than 3mm. DO I have to correct my footprint to compensate for the width of the polygon  lines.

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    0 rachaelp over 10 years ago

    Hi Ahsan,

     

    Is the 3mm x 3mm square you are drawing for a surface mount pad? If so you need to use the SMD command instead. That will create a surface mount pad the correct size with solder resist and paste mask areas correctly defined and will correctly map to the pins in the symbol. Similarly if your capacitor is through hole use the PAD command.

     

    If you are just drawing the body of the part on the tPlace of tDocu layers then just don't worry about it as they are only for placement markers on the silk screen and the assembly drawing.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rachaelp
    0 rachaelp over 10 years ago

    Hi Ahsan,

     

    Is the 3mm x 3mm square you are drawing for a surface mount pad? If so you need to use the SMD command instead. That will create a surface mount pad the correct size with solder resist and paste mask areas correctly defined and will correctly map to the pins in the symbol. Similarly if your capacitor is through hole use the PAD command.

     

    If you are just drawing the body of the part on the tPlace of tDocu layers then just don't worry about it as they are only for placement markers on the silk screen and the assembly drawing.

     

    Best Regards,

     

    Rachael