Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC mains on a PCB ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 193 subscribers
  • Views 21318 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 10 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • anishkgt
    0 anishkgt over 10 years ago

    Thanks rachaelp for the suggested layout. I think i would go with the first one. i had to catch a plane earlier hence short replies and delay.

     

    Thanks guys for pointing out about R11, i've corrected it now.

    So as suggested by Rachel and the other have these in my cart now. What more would i need, i mean i have all working but the decouplers were something new.

    Ceramic Disc & Plate Capacitor, CC Series, 0.1 µF, ± 10%, Y5P, 50 V, Radial Leaded http://www.newark.com/on-semiconductor/1n5908g/tvs-diode-5w-5v-unidirectional/dp/42K2954

    TVS Diode, MOSORB Series, Unidirectional, 5 V, 8.5 V, Axial Leaded, 2 Pins http://www.newark.com/nxp/bt139-600-127/triac-sensitive-gate-16a-to-220ab/dp/70R3252

    Triac, 600 V, 70 mA, 5 W, 1.5 V, TO-220AB, 155 A

    COVER, PCB FUSE HOLDER, HTC
    FUSE HOLDER, 5X20MM, HTC, PCB

     

    So i read someone mentioning about EMI filters, how necessary would these be for my design ? limited space on the board so trying to keep the overall components less.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • anishkgt
    0 anishkgt over 10 years ago

    Thanks rachaelp for the suggested layout. I think i would go with the first one. i had to catch a plane earlier hence short replies and delay.

     

    Thanks guys for pointing out about R11, i've corrected it now.

    So as suggested by Rachel and the other have these in my cart now. What more would i need, i mean i have all working but the decouplers were something new.

    Ceramic Disc & Plate Capacitor, CC Series, 0.1 µF, ± 10%, Y5P, 50 V, Radial Leaded http://www.newark.com/on-semiconductor/1n5908g/tvs-diode-5w-5v-unidirectional/dp/42K2954

    TVS Diode, MOSORB Series, Unidirectional, 5 V, 8.5 V, Axial Leaded, 2 Pins http://www.newark.com/nxp/bt139-600-127/triac-sensitive-gate-16a-to-220ab/dp/70R3252

    Triac, 600 V, 70 mA, 5 W, 1.5 V, TO-220AB, 155 A

    COVER, PCB FUSE HOLDER, HTC
    FUSE HOLDER, 5X20MM, HTC, PCB

     

    So i read someone mentioning about EMI filters, how necessary would these be for my design ? limited space on the board so trying to keep the overall components less.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    George Thomas wrote:

     

    Thanks rachaelp for the suggested layout. I think i would go with the first one. i had to catch a plane earlier hence short replies and delay.

    I actually think the latest one works better in some ways and it does give more options on connector type as it can cope with horizontal entry. You could even go for screw terminal type connectors right on the board so there weren't any removable connector plugs which for this, which I assume will be mounted inside a chassis, I think would be preferable.

    George Thomas wrote:

     

    So i read someone mentioning about EMI filters, how necessary would these be for my design ? limited space on the board so trying to keep the overall components less.

    Again assuming you have this in a chassis then you could have a filtered mains inlet IEC connector.

     

    More important than EMI filtering though is circuit protection from surges. I'd at the very least put a bi-directional TVS with a suitable standoff voltage across the AC input. Then if there is a surge on the line (surges can be many kVolts) this will clamp the voltage at a the specified clamp voltage and absorb energy until your inline fuse (in your inlet IEC connector or mains plug) blows from the increased current (which it will increase sharply once the TVS clamps).

     

    Take a look here for a range of possible devices: http://www.littelfuse.com/products/tvs-diodes/leaded.aspx

     

    Best Regards,

     

    Rachael