Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC mains on a PCB ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 193 subscribers
  • Views 21305 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 10 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • anishkgt
    0 anishkgt over 10 years ago

    came across this Spot welder controller from the web and he seem to be using tvs diodes as well. Why two thrustirs to control the load and am trouble witching on yhe Triac.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • anishkgt
    0 anishkgt over 10 years ago

    came across this Spot welder controller from the web and he seem to be using tvs diodes as well. Why two thrustirs to control the load and am trouble witching on yhe Triac.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 11/09/16 12:02, George Thomas wrote:

    Why two thrustirs to control the load and am trouble witching on yhe Triac.

     

    Triacs can suffer commutation problems with certain types of load -

    highly inductive (like a transformer) is one of the problem cases. The

    problem exhibits as a failure to turn off at the end of a half-cycle. I

    think this is more of an issue when PWMing the mains (light dimmer

    style), which is why I asked that question earlier. For that type of

    application a pair of back-to-back thyristors is more robust.

     

    It may not matter for your application if you occasionally get an extra

    half-cycle (10ms) as long as that is all you suffer. If you find that

    you get worse than that, the two-thyristor design is what you need.

     

    http://link.springer.com/chapter/10.1007%2F978-1-4612-9877-9_12 is worth

    reading on this.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer