Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC mains on a PCB ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 193 subscribers
  • Views 21292 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 10 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • anishkgt
    0 anishkgt over 10 years ago

    Hi rachaelp

     

    I think I've got the layout to somewhere closer to what you've provided earlier. Could not find a better route for the track from IC4 to IC1

     

    image

    Update:

    The pin on IC1 from IC4 has to be the same as it is an Interrupt pin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • anishkgt
    0 anishkgt over 10 years ago

    Hi rachaelp

     

    I think I've got the layout to somewhere closer to what you've provided earlier. Could not find a better route for the track from IC4 to IC1

     

    image

    Update:

    The pin on IC1 from IC4 has to be the same as it is an Interrupt pin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to anishkgt

    You've let that track from IC4 to IC1 break all the clearance rules again - the mains to signal clearance is an absolute requirement - no layout that breaks it is acceptable, ever.

     

    Put a resistor between IC4 and IC1 (or a link) if you can't find a better route. Don't be tempted to move the crystal further from IC1 - it's already too far from it. I think your processor is an Atmel AVR - it doesn't say on the schematic  - if so then take care with the crystal connections because AVRs are sensitive to noise picked up on the oscillator pins. I would rotate C7 by 90degrees and move the crystal closer to IC1.

     

    MK