Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC mains on a PCB ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 193 subscribers
  • Views 21258 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 10 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • anishkgt
    0 anishkgt over 10 years ago

    Well i've got it now i guess. hard move the Rectifier and IC4 so added a resistor in series with IC1, adjusted the +5v supply coming to C5 and going to R12. can't actually test this unless am back home.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • anishkgt
    0 anishkgt over 10 years ago

    Well i've got it now i guess. hard move the Rectifier and IC4 so added a resistor in series with IC1, adjusted the +5v supply coming to C5 and going to R12. can't actually test this unless am back home.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    Hi George,

     

    I think you misunderstood the point of adding the resistor between IC1 and IC4. The point was so you could use the resistor as a physical bridge over the other traces which were in the way and causing you to have to route the trace around the houses, what you have done with it is not helping in this regard and you've had to carve up the 5V and reroute part of it with a very thin trace.

     

    Also, why have D1 and D4 become huge? Have you replaced these with the type of TVS we spoke about previously? That wasn't meant for these locations, it was meant for across the AC input.

     

    Finally, It's going to sound nit picky, but I don't like the traces as strange angles.

     

    Best Regards,

     

    Rachael