Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC mains on a PCB ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 193 subscribers
  • Views 21232 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 10 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • anishkgt
    0 anishkgt over 10 years ago

    Hmmmm hope this went well.

     

    image

    Update:

         Rachel the TVS used here are quite big in size, approximately 5mm hence the size in the layout.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago in reply to anishkgt

    added AC tvs and PTC

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • anishkgt
    0 anishkgt over 10 years ago in reply to anishkgt

    added AC tvs and PTC

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    George Thomas wrote:

     

    added AC tvs and PTC

    It looks like you have put the TVS in series with the AC input. This is not correct, it should go in parallel with it.

     

    George Thomas wrote:

     

    Update:

         Rachel the TVS used here are quite big in size, approximately 5mm hence the size in the layout.

     

    The TVS in those DC side locations don't need to be that big. The power rating of 1500W is excessive for where it's located so you could choose smaller ones if you were running out of space.

     

    Rachael wrote:

     

    Finally, It's going to sound nit picky, but I don't like the traces as strange angles.

    And now look at the strange angled trace from the '+' pin of B1 which is almost (possibly is) touching the '-' pin. If you don't route at ugly odd angles you wont do this. Use the right mouse button when in routing mode to cycle through the bend styles or use the buttons at the top and use the two 45 degree ones (hint: you need to use both 45 degree styles depending on which way you'd like it to route)

     

    Morten Leikvoll wrote:

     

    The design looks earthless (isoladed AC). I don't know if there are any compliance rules that says you need to do that, but the fact that the LOAD is ext to pcb, and you are probably exposing the LOAD AC contacts for spot welding, makes me thing you do need it. Maybe it even requires isolated high voltage there, which would make this design require an isolating 1:1 transformer in front.

     

    This is sensible advice, I believe I mentioned in earlier posts my concerns about the lack of an earth connection. It all comes back to safety.

     

    George Thomas wrote:

     

    My idea for the connector was this.

    So what happened to these connectors? It looks like you still have the old ones in the design?

     

    Best Regards,

     

    Rachael