Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC mains on a PCB ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 193 subscribers
  • Views 21232 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 10 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • anishkgt
    0 anishkgt over 10 years ago

    And now look at the strange angled trace from the '+' pin of B1 which is almost (possibly is) touching the '-' pin. If you don't route at ugly odd angles you wont do this. Use the right mouse button when in routing mode to cycle through the bend styles or use the buttons at the top and use the two 45 degree ones (hint: you need to use both 45 degree styles depending on which way you'd like it to route)

    How could i miss that i did notice it earlier but slipped it, changed it now. Thanks for that.

     

    I've replaced the TVS at the DC side to this and changed the AC side too.

     

    This is sensible advice, I believe I mentioned in earlier posts my concerns about the lack of an earth connection. It all comes back to safety.

    I did notice that suggestion and kept it to be done at the end. So would that go ? just connect it to the earth terminal from the mains ?

    image

    Update: rotated the C1 and C2 for a better route.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • anishkgt
    0 anishkgt over 10 years ago

    And now look at the strange angled trace from the '+' pin of B1 which is almost (possibly is) touching the '-' pin. If you don't route at ugly odd angles you wont do this. Use the right mouse button when in routing mode to cycle through the bend styles or use the buttons at the top and use the two 45 degree ones (hint: you need to use both 45 degree styles depending on which way you'd like it to route)

    How could i miss that i did notice it earlier but slipped it, changed it now. Thanks for that.

     

    I've replaced the TVS at the DC side to this and changed the AC side too.

     

    This is sensible advice, I believe I mentioned in earlier posts my concerns about the lack of an earth connection. It all comes back to safety.

    I did notice that suggestion and kept it to be done at the end. So would that go ? just connect it to the earth terminal from the mains ?

    image

    Update: rotated the C1 and C2 for a better route.