Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC mains on a PCB ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 193 subscribers
  • Views 21329 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 10 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    Ooops - looks like I accidentally hit the wrong reply button before...

     

    On 03/09/16 14:57, George Thomas wrote:

    A total newbie to eagle design and PCB fab. So plase bear with on my

    silly questions, trying to learn.

     

    I have pcb that is schematically completed with the layout. Before i

    start the fabrication process i need some expert advise if the

    components placed and the wires routed are ok for the ac mains and the

    others. The load here will be a transformer. The ac mains are 240VAC and

    all works well as designed in the schematic on a bread broad except for

    the load for which MOC3023 is yet to arrive from where i've ordered.

     

     

    You have a lot of traces running unnecessarily close to each other and

    to pads. That's fine to low voltage stuff but undesirable when high

    voltages are present.

     

    Your placement of parts results in quite a few traces being quite long.

    That's undesirable in all domains. I particularly note that the trace

    from C7 to R20/21 goes all around the houses, when a simple rotation of

    C7 could reduce it to nothing.

     

    I don't know how much current that BTA08 is expected to drive, but the

    text describing the board as a "spot welder microcontroller" hints that

    you might be looking at several amps. If so, your traces look rather

    thin to me, especially given how long they are.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago in reply to autodeskguest

    Thanks a lot to take the effort to correct me.

     

    I've removed C7 and R21 which are actually used to protect the optocoupler but i don't see they being necessary here and i have rearranged the the remaining too.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 04/09/16 00:19, George Thomas wrote:

    Thanks a lot to take the effort to correct me.

     

    I've removed C7 and R21 which are actually used to protect the optocoupler but i don't see they being necessary here and i have rearranged the the remaining too.

     

    Definitely better... but I still think you want more "meat" on the

    important tracks.

     

    So, thinking about your design, it seems to me that the crucial part -

    the bit you need to worry about - is the path through the triac and

    between the connectors. That's where ALL the current is flowing - the

    rest is negligible. So, if it were my design, I'd start by placing

    those three components close together for optimal (i.e. very short)

    tracks. Then I'd make those tracks as wide as I could reasonably

    achieve. The rest can then fit around that.

     

    Also, the track from IC5 to R20 may be a low current track but it's at

    mains voltage. I'd rotate R20 to keep that track away from the low

    voltage ground plane.

     

    Would I be right in thinking you're using the triac as a pure switch?

    That is, you're either triggering it as early in the cycle as possible

    or not at all? I only mention it because I have some experience of

    driving a transformer in "light dimmer" mode (PWM of the mains cycle)

    and it's... tricky.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago in reply to rachaelp

    Well i hope this layout is what you guys suggested. When you said pitch is it the distance between the two terminals of the connector ? well on the physical connector it is 4.6mm

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    George Thomas wrote:

     

    you mean pinswap, right ? well that would again make the other trace longer, wouldn't it.

    I believe that's what was meant. It will lengthen the shorter trace slightly but shorten the other a lot more and stop it having to run around and under the transformer to get to the desired pin. You also need to make more space to get clearance between the two traces, you really don't have enough around the connectors. What is the pin pitch of your mains connectors, is it sufficient or do they need changing? Looking at the input on a typical 240V PSU I have here, the pitch on the input connector is 3.96mm. If you look at the clearance between the pads with connectors of this pitch you'll see that it's several mm. You should use this as a guide as to the minimum clearance between mains conductors and also their clearance to anything else. The advice Joern gave for moving parts and rerouting traces above is all valid and is what I would also suggest.

     

    Best regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago in reply to autodeskguest

    you mean pinswap, right ? well that would again make the other trace longer, wouldn't it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago in reply to autodeskguest

    yea ! your right. That was un-ticked all the while. Ticking it would pour more copper in those empty spaces under IC1.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 06/09/16 17:47, George Thomas wrote:

    so talking about removing floating copper, how can it be done manually ? tried to find it but could not.

     

    Assuming you mean how to avoid the unconnected bits on an Eagle board

    design, the trick is to turn the "orphans" setting OFF on the polygon.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 10 years ago in reply to anishkgt

    The way to take a little foil off of a pc-board is to slice through it with a sharp, newish pen-knife and then heat up the foil one wants to remove with a soldering iron and scrape it away.  The adhesive usually melts precipitantly.

     

    As an aside, the colored boards have a top anti-static layer, sometimes it is important to scrape this away between op-amp inputs. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago in reply to MattyLad

    so talking about removing floating copper, how can it be done manually ? tried to find it but could not. So I checked the creepage table and to me it was so much unfamiliar terms and French. I managed to learn that 8mm is the minimum distance between AC and DC that needs to be kept. other than that nothing.

     

    Would anyone be knowing a simpler document that I could read.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to MattyLad

    Am 06.09.2016 um 17:08 schrieb MattyLad:

    Looking better on the mains side, although I would still make the tracks to IC 5 thicker - just for durability.

     

    Please review your ground connections, you have some that go through very thin slivers.

    Also under the big IC you have floating copper (not connected to anything).

    A poor return will make your board bad for EMC also.

     

    Matt.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/205233

     

     

    Actually I didn't want to cut in here, but I don't like your AC section

    at all.

    Distances on terminals are usually just above the minimums.

    With your track from transformer pin5 to the AC terminal you lessen the

    distance to the second AC terminal pin.

    Although the rule says the shorter the better for large currents it

    doesn't say to forget the minimum distances image

    I would:

    1. exchange the transformer pins 1/5

    2. move R22 right above R20

    3. move the triac about half way between the terminals and R22

    4. move your tracks straight away from the terminals to get a save

    distance before turn towards the triac pins.

    5. The trigger line should go a little straight away from the triac

    before turning towards the optocoupler.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • MattyLad
    0 MattyLad over 10 years ago in reply to anishkgt

    Looking better on the mains side, although I would still make the tracks to IC 5 thicker - just for durability.

     

    Please review your ground connections, you have some that go through very thin slivers.

    Also under the big IC you have floating copper (not connected to anything).

    A poor return will make your board bad for EMC also.

     

    Matt.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    Hi George,

     

    It looks like you're really learning a lot with this design and you've had lots of good advice from people on this thread already and the difference between the initial version you posted and this latest version is quite substantial. I do wonder if the placement of the connectors, transformer etc could be rearranged such that the AC traces flow much straighter into the transformer, it's hard to see when you don't have the actual design files to experiment on but I think there is scope for further improvement there. I do also wonder if some of your clearances between conductors, for example around the connectors, are a little small. It might also be worth looking at some reference designs for mains power supply circuits to see how they deal with things like EMI filtering, circuit protection and most importantly safety.

     

    The latter is something I can't stress enough. Do your own research and ensure that your circuit, how it's fitted into your final design, and the system as a whole work together to ensure neither you, nor anybody else, can hurt themselves. Sorry if that sounds a little nannying but as you are new to circuit design and you're jumping straight into a mains powered product it probably should be said. All the advice people can give you here is great but you need to do your own research and ensure that what you finally make is safe and this is entirely your own responsibility.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    Hi George,

     

    It looks like you're really learning a lot with this design and you've had lots of good advice from people on this thread already and the difference between the initial version you posted and this latest version is quite substantial. I do wonder if the placement of the connectors, transformer etc could be rearranged such that the AC traces flow much straighter into the transformer, it's hard to see when you don't have the actual design files to experiment on but I think there is scope for further improvement there. I do also wonder if some of your clearances between conductors, for example around the connectors, are a little small. It might also be worth looking at some reference designs for mains power supply circuits to see how they deal with things like EMI filtering, circuit protection and most importantly safety.

     

    The latter is something I can't stress enough. Do your own research and ensure that your circuit, how it's fitted into your final design, and the system as a whole work together to ensure neither you, nor anybody else, can hurt themselves. Sorry if that sounds a little nannying but as you are new to circuit design and you're jumping straight into a mains powered product it probably should be said. All the advice people can give you here is great but you need to do your own research and ensure that what you finally make is safe and this is entirely your own responsibility.

     

    Best Regards,

     

    Rachael