Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC mains on a PCB ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 193 subscribers
  • Views 21258 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 10 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    Ooops - looks like I accidentally hit the wrong reply button before...

     

    On 03/09/16 14:57, George Thomas wrote:

    A total newbie to eagle design and PCB fab. So plase bear with on my

    silly questions, trying to learn.

     

    I have pcb that is schematically completed with the layout. Before i

    start the fabrication process i need some expert advise if the

    components placed and the wires routed are ok for the ac mains and the

    others. The load here will be a transformer. The ac mains are 240VAC and

    all works well as designed in the schematic on a bread broad except for

    the load for which MOC3023 is yet to arrive from where i've ordered.

     

     

    You have a lot of traces running unnecessarily close to each other and

    to pads. That's fine to low voltage stuff but undesirable when high

    voltages are present.

     

    Your placement of parts results in quite a few traces being quite long.

    That's undesirable in all domains. I particularly note that the trace

    from C7 to R20/21 goes all around the houses, when a simple rotation of

    C7 could reduce it to nothing.

     

    I don't know how much current that BTA08 is expected to drive, but the

    text describing the board as a "spot welder microcontroller" hints that

    you might be looking at several amps. If so, your traces look rather

    thin to me, especially given how long they are.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago in reply to autodeskguest

    Thanks a lot to take the effort to correct me.

     

    I've removed C7 and R21 which are actually used to protect the optocoupler but i don't see they being necessary here and i have rearranged the the remaining too.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 04/09/16 00:19, George Thomas wrote:

    Thanks a lot to take the effort to correct me.

     

    I've removed C7 and R21 which are actually used to protect the optocoupler but i don't see they being necessary here and i have rearranged the the remaining too.

     

    Definitely better... but I still think you want more "meat" on the

    important tracks.

     

    So, thinking about your design, it seems to me that the crucial part -

    the bit you need to worry about - is the path through the triac and

    between the connectors. That's where ALL the current is flowing - the

    rest is negligible. So, if it were my design, I'd start by placing

    those three components close together for optimal (i.e. very short)

    tracks. Then I'd make those tracks as wide as I could reasonably

    achieve. The rest can then fit around that.

     

    Also, the track from IC5 to R20 may be a low current track but it's at

    mains voltage. I'd rotate R20 to keep that track away from the low

    voltage ground plane.

     

    Would I be right in thinking you're using the triac as a pure switch?

    That is, you're either triggering it as early in the cycle as possible

    or not at all? I only mention it because I have some experience of

    driving a transformer in "light dimmer" mode (PWM of the mains cycle)

    and it's... tricky.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to rachaelp

    Am 07.09.2016 um 11:25 schrieb rachaelp:

    Joern Paschedag wrote:

     

    I don't know how others feel but imo was the layout from 06.09. much better.

    Yes I agree with you, as I said in one of my posts, the earlier layout in general was far better, while the routing to the transformer is improved a little, this one takes a big step backwards with regards the AC/DC isolation barrier. I'm also not happy with clearances between and to the mains voltage traces still and I think the mains connectors probably need to be changed to be a wider pitch to facilitate this.

     

    Best Regards,

     

    Rachael

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/205279

     

     

    I fully agree with you. Unfortunately there is no grid, so that one

    could measure the distance at the mains connectors and I hope those

    connectors are licensed for the 250VAC image

     

    Problem is, sometimes people don't follow the advice or sometimes the do

    too much image

    Well *** happenz image

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to autodeskguest

    Joern Paschedag wrote:

     

    I don't know how others feel but imo was the layout from 06.09. much better.

    Yes I agree with you, as I said in one of my posts, the earlier layout in general was far better, while the routing to the transformer is improved a little, this one takes a big step backwards with regards the AC/DC isolation barrier. I'm also not happy with clearances between and to the mains voltage traces still and I think the mains connectors probably need to be changed to be a wider pitch to facilitate this.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    Am 07.09.2016 um 08:28 schrieb George Thomas:

    you mean pinswap, right ? well that would again make the other trace longer, wouldn't it.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/205268

     

     

    Yes, but nobody requested you to turn the AC equipment by 90 degrees image

    If you place the eagle file here to where I gave my suggestion 06.09. I

    will change it  to what I meant.

    Imo your layout from 07.09. has decreased. Why do you think are the pins

    of the triac are so far spaced?

    Also on this new layout the optocoupler is awful.Why do you change so

    many things at all.

    Do only change the things people suggesting. I don't know how others

    feel but imo was the layout from 06.09. much better.

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to rachaelp

    On 07.09.2016 10:53, rachaelp wrote:

    Morten Leikvoll wrote:

     

    Also, make sure its fire- and explosion-proof in case something should short circuit, or you get struck by lightning at the AC. I saw someone mentioning fuse, and I assume you have one at the AC inlet, prior to entering the pcb.

    Yes absolutely! The fuse in the mains plug probably isn't enough to protect the circuit though as it may be over rated and won't necessarily blow quickly enough. I'd consider adding a PTC and MOV's and/or TVS diodes as surge protection if this were my design. I'd also add some EMI filtering and have the earth connected in too.

     

    Best Regards,

     

    Rachael

     

    Fuse in the mains plug? image That is UK-specific I guess. Either use IEC

    power inlet with embedded fuse (like farnell 1516059), or make sure the

    first thing the power line meets, is a fuse. (And ground meets the metal

    box).

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to rachaelp

    Morten Leikvoll wrote:

     

    Also, make sure its fire- and explosion-proof in case something should short circuit, or you get struck by lightning at the AC. I saw someone mentioning fuse, and I assume you have one at the AC inlet, prior to entering the pcb.

    Yes absolutely! The fuse in the mains plug probably isn't enough to protect the circuit though as it may be over rated and won't necessarily blow quickly enough. I'd consider adding a PTC and MOV's and/or TVS diodes as surge protection if this were my design. I'd also add some EMI filtering and have the earth connected in too.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    George Thomas wrote:

     

    Hmmmm knew there was something wrong when autorouting was completing at 100% for all the efforts . So is there any option to avoid traces under or near IC's and opto-couplers and where else should i avoid traces, caps ?

    Yes, you can use the restrict layers to specify where traces are not allowed to go. Take a look at this article for a quick guide on how to do this: http://dangerousprototypes.com/blog/2012/08/08/how-to-eagle-keepout-and-restrict-layers/

     

    In general however, a lot of auto-router issues stem from deficiencies in the initial placement. With any routing job, manual or auto, but especially with auto routing, the placement will make or break the layout. Your latest placement has a number of issues, a few of which I highlighted in my previous post. You need to take a step back and think about how the circuit "flows" and try and place things to keep the flow simple.

     

    If I were you I would consider doing at least some of the more critical routing manually and leave the auto router for the less critical stuff. Also, don't just hit the autoroute button and let it do it's thing in one go, tell it to route specific smaller groups of more important signals first, inspect them and manually tweak if needed and then move on to the next. Breaking it down in this way and keeping an eye on how it is doing will give you a better chance of success.

     

    Jorge Garcia wrote a good blog post on the auto router a while back which is worth a read: https://www.element14.com/community/community/cadsoft_eagle/blog/2015/06/17/are-you-better-than-the-autorouter

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 06.09.2016 22:43, George Thomas wrote:

    yea ! your right. That was un-ticked all the while. Ticking it would pour more copper in those empty spaces under IC1.

     

     

    Dont forget those shielded holes in the corner.. I suppose you do want

    to put this pcb down in a box? Maybe even shielded metal box? image

     

    Interesting project. Without reading it all, I hope you have dimensioned

    the AC-LOAD wires for those high currents.

     

    Also, even if this is out of my experience field, I would take an extra

    look at this high current current loop. You don't want an EMP generator

    image For example, I would route the pulsed load pin direct to the AC

    input, not passing the transformer first. This will narrow the loop, and

    also avoid spikes at the transformer due to voltage loss during current

    pulses.

     

    Also, make sure its fire- and explosion-proof in case something should

    short circuit, or you get struck by lightning at the AC. I saw someone

    mentioning fuse, and I assume you have one at the AC inlet, prior to

    entering the pcb.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 06.09.2016 22:43, George Thomas wrote:

    yea ! your right. That was un-ticked all the while. Ticking it would pour more copper in those empty spaces under IC1.

     

     

    Dont forget those shielded holes in the corner.. I suppose you do want

    to put this pcb down in a box? Maybe even shielded metal box? image

     

    Interesting project. Without reading it all, I hope you have dimensioned

    the AC-LOAD wires for those high currents.

     

    Also, even if this is out of my experience field, I would take an extra

    look at this high current current loop. You don't want an EMP generator

    image For example, I would route the pulsed load pin direct to the AC

    input, not passing the transformer first. This will narrow the loop, and

    also avoid spikes at the transformer due to voltage loss during current

    pulses.

     

    Also, make sure its fire- and explosion-proof in case something should

    short circuit, or you get struck by lightning at the AC. I saw someone

    mentioning fuse, and I assume you have one at the AC inlet, prior to

    entering the pcb.