Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How to flip a component on pcb and stay on same side
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 22 replies
  • Answers 1 answer
  • Subscribers 190 subscribers
  • Views 5671 views
  • Users 0 members are here
Related

How to flip a component on pcb and stay on same side

e14 Contributor
e14 Contributor over 10 years ago

I have a radial electrolytic capacitor component that lays down on its side. If say it is upright (pins on bottom) and capacitor is bent down, with + on left and - on right.  So now how do I flip it so - is on left and + is on right but capacitor is still upright (pins still on bottom).

Placing it on the other side won't work, as the silkscreen will be on the wrong side.

 

You can flip component on schematic (for the same reason to reverse the order of pins), but how do you do it  on pcb?

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    0 rachaelp over 10 years ago

    So what you are saying is you have a custom radial part with the silk screen drawn such that is shows the body of the part as it would be with the leads formed to 90 degrees so you can lie it down? I.e. so simple rotation isn't going to work?

     

    If this is the case I think you need to create an alternative package with your pins the opposite way round so you can then add this to the part as a variant and select it in the board by right clicking and selecting "Package" from the menu. Then you choose your alternative package from the list.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to rachaelp

    Am 04.09.2016 um 12:32 schrieb rachaelp:

    So what you are saying is you have a custom radial part with the silk screen drawn such that is shows the body of the part as it would be with the leads formed to 90 degrees so you can lie it down? I.e. so simple rotation isn't going to work?

     

    If this is the case I think you need to create an alternative package with your pins the opposite way round so you can then add this to the part as a variant and select it in the board by right clicking and selecting "Package" from the menu. Then you choose your alternative package from the list.

     

    Best Regards,

     

    Rachael

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/205093

     

     

    As far as I understand what you want is to ROTATE a device (turn it but

    stay on the same side).

    Use the MOVE command, grab the device and then right click it with  the

    mouse. Every (right) click rotates it by 90 degrees. If you want a

    different angle use the rotate command. Help rotate.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to autodeskguest

    Nope. If you rotate the radial capacitor laying down, the leads will switch, but it would be laying down in the opposite direction, which is not what I want.

     

    FWIW, adding a variant did not seem to work. Whatever edit I do reflects on the other variants of the same package, which is weird. So I just ended up adding a new package.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to e14 Contributor

    On 05/09/16 19:12, Jerry Sy wrote:

    I think you need to look outside your little bubble. lol.

     

    Well!

     

    I have been very polite and helpful to you because I'd assumed you were

    a genuine person looking for help past a slight block. But if you're

    going to respond by being rude then I will certainly not be helping any

    further.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to e14 Contributor

    Am 05.09.2016 um 20:12 schrieb Jerry Sy:

    not to me and a lot of others.

     

    OK Buster. It is Ok if you speak for  yourself but imho you do not speak

    not for others.

    Those "others" may speak for themselves if they want to.

    And last but not least you don't speak for me. Get that behind your ears.

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to autodeskguest

    not to me and a lot of others.

    The fact that if you do a search you will find numerous results discussing this same thing is proof positive this is not intuitive.

    I think you need to look outside your little bubble. lol.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rachaelp

    Thanks for the explanation. Now I understand. and the confusion stems from the interchangeable usage of package and variant.

     

    When one looks at the UI, you see one column called package and a second column called variant.

    When you say add a new variant, the obvious intuitive action is to add a variant to the package.

    It will be less confusing to just say add a new package to the device, then one will right click to add a new package.

     

    since a package is automatically associated with a variant, I suppose that is where the parlance of add a variant originated from. But since the way the UI is presented distinguishes package and variant, one would add a variant to the package rather than add a new package (with the associated new variant) to the device.

     

    I hope thread clears up any confusion in the future for anyone searching to find answers and lands on this thread.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to e14 Contributor

    Rachael and Olin have both answered this in their own, respective,

    inimitable ways image However...

     

    On 05/09/16 08:22, Jerry Sy wrote:

    It is not intuitive.

    Not to you but it seems quite natural to some others.

     

     

    Device A

    Package A variant ""

    Package B variant B1

    Package B variant B2

    Package B variant B3

     

    The way you've written this table clearly illustrates the incorrect

    mindset that makes it seem "not intuitive" to you. As I tried to explain

    before, the correct way to write this is:

     

    Device A

       Variant ""   -> Package A

       Variant B1   -> Package B

    etc.

     

    The point is, Variant is a parameter of the DEVICE and NOT of the

    PACKAGE. Get that fact understood and all of the supposed weirdness just

    floats away.

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to e14 Contributor

    Jerry Sy wrote on Mon, 05 September 2016 03:22

    Device A

    Package A variant ""

    Package B variant B1

    Package B variant B2

    Package B variant B3

     

    If you edit B3, the same change appears in B1 and B2.

     

     

    No.  You edited B, not B3, so of course variants B1-B3 changed.  Stop and

    actually  think how device definitions work before flailing around or

    delcaring it stupid.

     

    Each device in a library is a set of bindings between a symbol (what goes

    in the schematic) and a package (what goes on the board).  The binding

    includes information like what pins of the symbol represent what physical

    pads of the package.  Each such binding is called a "variant".  This refers

    to a variant of the device, not any package or symbol.  The various

    bindings within a device need to be uniquely labeled somehow.  That somehow

    is the variant name.

     

    Devices can currently only refer to a single symbol, but each variant can

    reference any suitable package in that library.  Note that devices

    reference symbols and packages.  The symbol and package definitions exist

    separately in that library.  If you edit a symbol or package, all device

    variants within all devices in that library referencing that symbol or

    package will change.

     

    If you want two different packages, you have to make two different

    packages.  Then you can point two (or more) variants to those packages to

    use them.  This is what you want.  A package defines physical layout.  You

    want two layouts that are different from each other, so you have to make

    two packages.  Once you do that, you edit the device that references the

    original package and add a variant to reference the new package.  When you

    go to add the device to the schematic, you have to chose between all the

    variants in the package to decide which one you want to use this time.

     

    Think about it.  This works the way you want it to work and pretty much the

    way it has to work.  Bindings are references and don't contain copies of

    what they are binding in their own private hidey-hole somewhere.  You

    wouldn't want them too.  That would make fixing or enhancing a package a

    mess because you'd have to track down all the bindings that use the package

    and fix all the separate copies.

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to e14 Contributor

    I think Rob has explained where things got a bit confused quite well so I wont rehash his explanation. In your situation creating package C was the correct things to do. It's still a variant within the device, but it's a variant with a different package.

     

    In the case above where you have package B pointing to variants B1, B2, B3, a use case for this could be if you have say a standard symbol for an NPN transistor and a SOT-23 package and you create a generic NPN component using these, then there are several combinations of pinouts possible for connecting B,C and E of the symbol to pins 1, 2 and 3 of the package. You use the variants to change the mapping of the symbol pins to the package pads. So in the terminology you gave above:

     

    Device NPN

    Package SOT-23 variant CBE // Maps pin 1 -> C, 2 -> B, 3 -> E

    Package SOT-23 variant BCE // Maps pin 2 -> B, 2 -> C, 3 -> E

    etc....

     

    Note, this is not how I do transistors in my libraries but this is an example of how you could use the package variants in a useful way how you were trying to do.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rachaelp
    0 rachaelp over 10 years ago in reply to e14 Contributor

    I think Rob has explained where things got a bit confused quite well so I wont rehash his explanation. In your situation creating package C was the correct things to do. It's still a variant within the device, but it's a variant with a different package.

     

    In the case above where you have package B pointing to variants B1, B2, B3, a use case for this could be if you have say a standard symbol for an NPN transistor and a SOT-23 package and you create a generic NPN component using these, then there are several combinations of pinouts possible for connecting B,C and E of the symbol to pins 1, 2 and 3 of the package. You use the variants to change the mapping of the symbol pins to the package pads. So in the terminology you gave above:

     

    Device NPN

    Package SOT-23 variant CBE // Maps pin 1 -> C, 2 -> B, 3 -> E

    Package SOT-23 variant BCE // Maps pin 2 -> B, 2 -> C, 3 -> E

    etc....

     

    Note, this is not how I do transistors in my libraries but this is an example of how you could use the package variants in a useful way how you were trying to do.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rachaelp

    Thanks for the explanation. Now I understand. and the confusion stems from the interchangeable usage of package and variant.

     

    When one looks at the UI, you see one column called package and a second column called variant.

    When you say add a new variant, the obvious intuitive action is to add a variant to the package.

    It will be less confusing to just say add a new package to the device, then one will right click to add a new package.

     

    since a package is automatically associated with a variant, I suppose that is where the parlance of add a variant originated from. But since the way the UI is presented distinguishes package and variant, one would add a variant to the package rather than add a new package (with the associated new variant) to the device.

     

    I hope thread clears up any confusion in the future for anyone searching to find answers and lands on this thread.