Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) CA3046 splitting pins
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 670 views
  • Users 0 members are here
Related

CA3046 splitting pins

seyfullahgokduman
seyfullahgokduman over 10 years ago

Guys hello.Im trying to add the CA3046 like in the picture below but i can not handle it.anyone can help me?how can i draw this ?

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • seyfullahgokduman
    0 seyfullahgokduman over 10 years ago

    sorry guys im gonna try to be more clear.as you see in the first picture,1,2and 3 pins connected to the 4 and 5 pin.i want to split 1,2 and 3 pins from them.so i want to connect them like in the second picture.

    rachaelp shabaz

    Attachments:
    image
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • seyfullahgokduman
    0 seyfullahgokduman over 10 years ago

    sorry guys im gonna try to be more clear.as you see in the first picture,1,2and 3 pins connected to the 4 and 5 pin.i want to split 1,2 and 3 pins from them.so i want to connect them like in the second picture.

    rachaelp shabaz

    Attachments:
    image
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to seyfullahgokduman

    Seyfullah Gökduman wrote:

    sorry guys im gonna try to be more clear.as you see in the first

    picture,1,2and 3 pins connected to the 4 and 5 pin.i want to split 1,2

    and 3 pins from them.so i want to connect them like in the second

    picture.

     

    I'm still not sure what you mean ... but I guess you would like to

    split the T1-T2 symbol into two separate ones.

     

    That is, in this case, not possible because T1 and T2 share pin 3.

    And that is - as Rachael already told you - not possible, because

    eagle can't connect more than one symbol pin to one package pad.

    --

     

    Lorenz