Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Complete but incomplete?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 189 subscribers
  • Views 1593 views
  • Users 0 members are here
  • airwires
  • air wires
  • airwire
  • unconnected
Related

Complete but incomplete?

tomstorey
tomstorey over 10 years ago

Working on a PCB design, and Ive completed  the layout, but Eagle is telling me there are seemingly some things that still need to be done.

 

Take the attached screen shot for example. Ive selected a net, which highlights all of the nearby pads/traces etc that are part of it. But there are airwires telling me I still need to connect something?

 

Can anyone tell me why this would be happening, and perhaps how I can get rid of them (short of connecting them the way it thinks I should, which would spoil my design.) image

 

Thanks!

 

image

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 07/09/16 17:59, Tom Storey wrote:

    Working on a PCB design, and Ive completed  the layout, but Eagle is telling me there are seemingly some things that still need to be done.

     

    Take the attached screen shot for example. Ive selected a net, which highlights all of the nearby pads/traces etc that are part of it. But there are airwires telling me I still need to connect something?

     

    Can anyone tell me why this would be happening, and perhaps how I can get rid of them (short of connecting them the way it thinks I should, which would spoil my design.) image

     

    Thanks!

     

    I assume you mean that your intent was to have multiple copies of the

    same circuit, and your problem is that Eagle wants to connect them all

    together? If so, the cause is almost certainly that you copied blocks of

    schematic which had named nets. The names are retained in the copy,

    which tells Eagle they are the same net (that's how you connect nets

    between sheets, for example). You need to go back to the schematic and

    rename the problematic net segments to be different.

     

    Note that any net connected to a supply symbol is inherently named by

    that connection. If you want your multiple circuits to have independent

    power connections then you have to do more work.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 07/09/16 17:59, Tom Storey wrote:

    Working on a PCB design, and Ive completed  the layout, but Eagle is telling me there are seemingly some things that still need to be done.

     

    Take the attached screen shot for example. Ive selected a net, which highlights all of the nearby pads/traces etc that are part of it. But there are airwires telling me I still need to connect something?

     

    Can anyone tell me why this would be happening, and perhaps how I can get rid of them (short of connecting them the way it thinks I should, which would spoil my design.) image

     

    Thanks!

     

    I assume you mean that your intent was to have multiple copies of the

    same circuit, and your problem is that Eagle wants to connect them all

    together? If so, the cause is almost certainly that you copied blocks of

    schematic which had named nets. The names are retained in the copy,

    which tells Eagle they are the same net (that's how you connect nets

    between sheets, for example). You need to go back to the schematic and

    rename the problematic net segments to be different.

     

    Note that any net connected to a supply symbol is inherently named by

    that connection. If you want your multiple circuits to have independent

    power connections then you have to do more work.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • tomstorey
    0 tomstorey over 10 years ago in reply to autodeskguest

    Indeed I did duplicate blocks of circuit in my schematic. In this case the parts in question all share the same net name on purpose (+5V in this case, and one between two pads/traces part of the GND net). But although I have connected them all together, and in the screenshot I have highlighted the net named +5V and it has highlighted everything correctly, its still telling me that I need to connect them together. It doesnt seem happy with the way Ive done it, even though it would appear to be valid.

     

    It all checks out in the gerbers that I exported, so maybe its nothing to worry about. Just thought it would be nice to see a full board without any airwires left.