EAGLE User Support (English) Complete but incomplete?
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
  • State Not Answered
  • Replies 12 replies
  • Subscribers 181 subscribers
  • Views 1225 views
  • Users 0 members are here
  • airwires
  • air wires
  • airwire
  • unconnected
Related

Complete but incomplete?

tomstorey
tomstorey over 9 years ago

Working on a PCB design, and Ive completed  the layout, but Eagle is telling me there are seemingly some things that still need to be done.

 

Take the attached screen shot for example. Ive selected a net, which highlights all of the nearby pads/traces etc that are part of it. But there are airwires telling me I still need to connect something?

 

Can anyone tell me why this would be happening, and perhaps how I can get rid of them (short of connecting them the way it thinks I should, which would spoil my design.) image

 

Thanks!

 

image

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 07/09/16 17:59, Tom Storey wrote:

    Working on a PCB design, and Ive completed  the layout, but Eagle is telling me there are seemingly some things that still need to be done.

     

    Take the attached screen shot for example. Ive selected a net, which highlights all of the nearby pads/traces etc that are part of it. But there are airwires telling me I still need to connect something?

     

    Can anyone tell me why this would be happening, and perhaps how I can get rid of them (short of connecting them the way it thinks I should, which would spoil my design.) image

     

    Thanks!

     

    I assume you mean that your intent was to have multiple copies of the

    same circuit, and your problem is that Eagle wants to connect them all

    together? If so, the cause is almost certainly that you copied blocks of

    schematic which had named nets. The names are retained in the copy,

    which tells Eagle they are the same net (that's how you connect nets

    between sheets, for example). You need to go back to the schematic and

    rename the problematic net segments to be different.

     

    Note that any net connected to a supply symbol is inherently named by

    that connection. If you want your multiple circuits to have independent

    power connections then you have to do more work.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tomstorey
    0 tomstorey over 9 years ago in reply to autodeskguest

    Indeed I did duplicate blocks of circuit in my schematic. In this case the parts in question all share the same net name on purpose (+5V in this case, and one between two pads/traces part of the GND net). But although I have connected them all together, and in the screenshot I have highlighted the net named +5V and it has highlighted everything correctly, its still telling me that I need to connect them together. It doesnt seem happy with the way Ive done it, even though it would appear to be valid.

     

    It all checks out in the gerbers that I exported, so maybe its nothing to worry about. Just thought it would be nice to see a full board without any airwires left.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to tomstorey

    On 07/09/16 19:01, Tom Storey wrote:

    Indeed I did duplicate blocks of circuit in my schematic. In this case the parts in question all share the same net name on purpose (+5V in this case, and one between two pads/traces part of the GND net). But although I have connected them all together, and in the screenshot I have highlighted the net named +5V and it has highlighted everything correctly, its still telling me that I need to connect them together. It doesnt seem happy with the way Ive done it, even though it would appear to be valid.

     

     

    Have you run RATSNEST on it? It's possible for unnecessary airwires to

    be left if you add copper other than by the "route" tool (or even if you

    route specific ways) but ratsnest forces a re-calculation.

     

    Alternatively (and this can be hidden by a ratsnest) there may be traces

    that overlap without actually joining. Eagle will consider that an

    incomplete track and will leave an airwire. After re-calc that tends to

    be a very short one that you'd easily miss...

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tomstorey
    0 tomstorey over 9 years ago in reply to autodeskguest

    Yup, have clicked ratsnest a million times while working in other areas of the board. image

     

    Theres nothing overlapping that would break or interfere with the continuity of a trace.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to tomstorey

    Tom Storey wrote:

     

    Yup, have clicked ratsnest a million times while working in other areas of the board.

     

    Theres nothing overlapping that would break or interfere with the continuity of a trace.

    Ahhh the old immortal air wire bug. I had a board once where a single air wire stayed despite all attempts to find some minor misconnection. There wasn't one. In the end I closed the schematic, renamed the board, created a new empty board with the old name, copied everything across from the old board the the new board, closed everything down and reopened the schematic and board together and hey presto the air wire was finally gone! I never did work out what triggered it to happen but I did get it fixed this way.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to rachaelp

    On 07/09/16 21:07, rachaelp wrote:

    Tom Storey wrote:

     

    Yup, have clicked ratsnest a million times while working in other areas of the board.

     

    Theres nothing overlapping that would break or interfere with the continuity of a trace.

    Ahhh the old immortal air wire bug. I had a board once where a single air wire stayed despite all attempts to find some minor misconnection. There wasn't one. In the end I closed the schematic, renamed the board, created a new empty board with the old name, copied everything across from the old board the the new board, closed everything down and reopened the schematic and board together and hey presto the air wire was finally gone! I never did work out what triggered it to happen but I did get it fixed this way.

     

    Ah... yes... there's a bug in V5 (don't know if the more recent ones fix

    it) that can leave invisible bits of unwanted trace on the board. They

    are associated with a net, so ratsnest adds an airwire to them, because

    they are unconnected to the rest of the net.

     

    That one didn't occur to me because the problem reported was not "a

    random airwire appears that ends in middle of nowhere", which is how the

    bug always seems to manifest for me.

     

    Anyway, the solution is simple - just rip up the offending stray bit of

    trace. At least, it would be simple if the said bit of trace weren't

    completely invisible! So far I've always managed to fix it by MOVEing

    one end of the invisible trace (at the stray end of the airwire) at

    which point the trace becomes visible and can be ripped up. It usually

    takes a few goes, though, because the trace isn't immediately visible to

    the MOVE command, either.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    On 07/09/16 21:07, rachaelp wrote:

    Tom Storey wrote:

     

    Yup, have clicked ratsnest a million times while working in other areas of the board.

     

    Theres nothing overlapping that would break or interfere with the continuity of a trace.

    Ahhh the old immortal air wire bug. I had a board once where a single air wire stayed despite all attempts to find some minor misconnection. There wasn't one. In the end I closed the schematic, renamed the board, created a new empty board with the old name, copied everything across from the old board the the new board, closed everything down and reopened the schematic and board together and hey presto the air wire was finally gone! I never did work out what triggered it to happen but I did get it fixed this way.

     

    Ah... yes... there's a bug in V5 (don't know if the more recent ones fix

    it) that can leave invisible bits of unwanted trace on the board. They

    are associated with a net, so ratsnest adds an airwire to them, because

    they are unconnected to the rest of the net.

     

    That one didn't occur to me because the problem reported was not "a

    random airwire appears that ends in middle of nowhere", which is how the

    bug always seems to manifest for me.

     

    Anyway, the solution is simple - just rip up the offending stray bit of

    trace. At least, it would be simple if the said bit of trace weren't

    completely invisible! So far I've always managed to fix it by MOVEing

    one end of the invisible trace (at the stray end of the airwire) at

    which point the trace becomes visible and can be ripped up. It usually

    takes a few goes, though, because the trace isn't immediately visible to

    the MOVE command, either.

     

     

     

    I think this was subtly different. I could get the pesky air wire to show in completely different parts of the net depending on how I ripped it all out and re-drew it. It was really really weird. In the end the only way I could find to sort it was to copy and paste everything to a new blank board and the rogue air wires were removed. Unfortunately I don't have a copy of the board in the state showing the issue anymore so I can't send it on to CADSoft to investigate.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to rachaelp

    Am 07.09.2016 um 23:12 schrieb rachaelp:

    CadSoft Guest wrote:

     

    On 07/09/16 21:07, rachaelp wrote:

    Tom Storey wrote:

     

    Yup, have clicked ratsnest a million times while working in other areas of the board.

     

    Theres nothing overlapping that would break or interfere with the continuity of a trace.

    Ahhh the old immortal air wire bug. I had a board once where a single air wire stayed despite all attempts to find some minor misconnection. There wasn't one. In the end I closed the schematic, renamed the board, created a new empty board with the old name, copied everything across from the old board the the new board, closed everything down and reopened the schematic and board together and hey presto the air wire was finally gone! I never did work out what triggered it to happen but I did get it fixed this way.

     

    Ah... yes... there's a bug in V5 (don't know if the more recent ones fix

    it) that can leave invisible bits of unwanted trace on the board. They

    are associated with a net, so ratsnest adds an airwire to them, because

    they are unconnected to the rest of the net.

     

    That one didn't occur to me because the problem reported was not "a

    random airwire appears that ends in middle of nowhere", which is how the

    bug always seems to manifest for me.

     

    Anyway, the solution is simple - just rip up the offending stray bit of

    trace. At least, it would be simple if the said bit of trace weren't

    completely invisible! So far I've always managed to fix it by MOVEing

    one end of the invisible trace (at the stray end of the airwire) at

    which point the trace becomes visible and can be ripped up. It usually

    takes a few goes, though, because the trace isn't immediately visible to

    the MOVE command, either.

     

     

     

    I think this was subtly different. I could get the pesky air wire to show in

    completely different parts of the net depending on how I ripped it all out and

    re-drew it. It was really really weird. In the end the only way I could find

    to sort it was to copy and paste everything to a new blank board and the rogue

    air wires were removed. Unfortunately I don't have a copy of the board in the

    state showing the issue anymore so I can't send it on to CADSoft to investigate.

     

     

     

    As Rachael wrote, feel free to send the board to support@cadsoft.de.

    So we can invsetigate.....

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to autodeskguest

    On 08/09/16 07:31, Richard Hammerl wrote:

     

    As Rachael wrote, feel free to send the board to support@cadsoft.de.

    So we can invsetigate.....

     

    I will try to remember to do so next time it happens, especially if I

    manage to get it on V7

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to autodeskguest

    On 08/09/16 07:49, Rob Pearce wrote:

    On 08/09/16 07:31, Richard Hammerl wrote:

     

    As Rachael wrote, feel free to send the board to support@cadsoft.de.

    So we can invsetigate.....

     

    I will try to remember to do so next time it happens, especially if I

    manage to get it on V7

     

    Sorry, meant to add, hopefully Tom still has his rogue to send now...

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>