Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Overlapping connector pins not connecting
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 188 subscribers
  • Views 1294 views
  • Users 0 members are here
Related

Overlapping connector pins not connecting

pars
pars over 10 years ago

Hi,

I did a brief search thru the forum but didn't see this asked already.

I am laying out a 2-sided board, and wanted to put 2 different connector footprints/pads/holes to allow the user to select which connector type to use. These are 3-pin Molex KK 0.100" and Phoenix 0.508" connectors. The center pin of each is connected to a top ground plane. In the past on commercial PCBs, I have manually added the Molex connectors in exactly this way, and they fit fine. There is also ample clearance between the pads for pins 1 and 3 of both connectors (no DRC errors).

 

If I superimpose the connectors on one another (same x-y location), the ground plane will not fill in the connection to either of these pads (2 airwires). If I move the connectors apart it works fine.

Any tips?

 

Also, I assume this might give DRC errors for drill distance? Can I just ignore those?

Thanks, and great forum!

Chris

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    Hi

    Make a small board with only those connectors and your polygon and post it

    here.

    With luck there will be enough information then to assist

     

    HTH

    Warren

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pars
    0 pars over 10 years ago in reply to autodeskguest

    Based on the feedback from Warren, I redid some things.

     

    1. Combo Molex/Phoenix connector part, so no double drilling with different bit sizes on the center pin.
    2. For the last point, I added rounded slots in the milling layer, as well as a rectangular copper pad on both top and bottom for the center pin overlap. Since the slot should be cut first, the drill problems shouldn't matter, but I am not as experienced with fabs as most of you are. Here is a pic of the board without the top layer. The fab that is going to run these does do plated slots, with a minimum dimension of 0.8mm. The rectangular slots for the 12 pins on the CP2500 are 3.2 x 0.8mm. The blades on these are either 3.0 x 0.4mm (older production) or 2.5 x 0.4mm (new production).

    image

     

     

    I had sent previous gerbers to the fab, but they have not commented yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • pars
    0 pars over 10 years ago in reply to autodeskguest

    Based on the feedback from Warren, I redid some things.

     

    1. Combo Molex/Phoenix connector part, so no double drilling with different bit sizes on the center pin.
    2. For the last point, I added rounded slots in the milling layer, as well as a rectangular copper pad on both top and bottom for the center pin overlap. Since the slot should be cut first, the drill problems shouldn't matter, but I am not as experienced with fabs as most of you are. Here is a pic of the board without the top layer. The fab that is going to run these does do plated slots, with a minimum dimension of 0.8mm. The rectangular slots for the 12 pins on the CP2500 are 3.2 x 0.8mm. The blades on these are either 3.0 x 0.4mm (older production) or 2.5 x 0.4mm (new production).

    image

     

     

    I had sent previous gerbers to the fab, but they have not commented yet.