Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Overlapping connector pins not connecting
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 188 subscribers
  • Views 1292 views
  • Users 0 members are here
Related

Overlapping connector pins not connecting

pars
pars over 10 years ago

Hi,

I did a brief search thru the forum but didn't see this asked already.

I am laying out a 2-sided board, and wanted to put 2 different connector footprints/pads/holes to allow the user to select which connector type to use. These are 3-pin Molex KK 0.100" and Phoenix 0.508" connectors. The center pin of each is connected to a top ground plane. In the past on commercial PCBs, I have manually added the Molex connectors in exactly this way, and they fit fine. There is also ample clearance between the pads for pins 1 and 3 of both connectors (no DRC errors).

 

If I superimpose the connectors on one another (same x-y location), the ground plane will not fill in the connection to either of these pads (2 airwires). If I move the connectors apart it works fine.

Any tips?

 

Also, I assume this might give DRC errors for drill distance? Can I just ignore those?

Thanks, and great forum!

Chris

  • Sign in to reply
  • Cancel
Parents
  • pars
    0 pars over 10 years ago

    Also I saw your post on Eagle central, but don't have posting permission there (yet).

    1. I had fixed the problems with connections in the schematic, but thanks.
    2. See above.
    3. Good idea on combining the connectors into one part, 5 pads. Done. If I don't replace the ones in my design with these, I will increase the drill size on the KK connector to match, so should make the fab happier.
    4. Not sure what to do on this one. The fab hasn't complained about this, but I would like to make things as easy as possible on them.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pars
    0 pars over 10 years ago in reply to pars

    One curious thing I found when doing this (in the con-molex library) was

    that the Molex KK connector package I was duplicating, there were 4 pads

    for a 3-pin connector. Pads 2 and 4 were superimposed on each other, with

    pad 4 not being connected in the device.

     

    Any reason a library would be done this way? Or just an oversight?

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • pars
    0 pars over 10 years ago in reply to pars

    One curious thing I found when doing this (in the con-molex library) was

    that the Molex KK connector package I was duplicating, there were 4 pads

    for a 3-pin connector. Pads 2 and 4 were superimposed on each other, with

    pad 4 not being connected in the device.

     

    Any reason a library would be done this way? Or just an oversight?

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to pars

    Chris Young wrote:

    One curious thing I found when doing this (in the con-molex library) was

    that the Molex KK connector package I was duplicating, there were 4 pads

    for a 3-pin connector. Pads 2 and 4 were superimposed on each other, with

    pad 4 not being connected in the device.

     

    Any reason a library would be done this way? Or just an oversight?

     

    most likely the latter.

     

    Never trust a library you haven't  botched yourself 8-)

    --

     

    Lorenz