Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Trying to add PLCC68 socket from the smd-special.lbr
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1613 views
  • Users 0 members are here
  • eagle
  • socket
  • plcc
Related

Trying to add PLCC68 socket from the smd-special.lbr

konsolkongen
konsolkongen over 10 years ago

Hi. I'm new to Eagle. I know the very basics of how to use it, but I have some problems adding a part to my board. I wan't to add a PLCC68 socket, which is included in the smd-special library. I just want the empty socked and I can wire up all the connections manually.

 

However, the socket cannot be found when in schematics mode, where I would normally add it. I can only find it when in board design, and there I'm not allowed to add it. I get the error "Can't backannotate this operation. Please do this in the schematic!", which as I said is not possible because the part does not show up there.

 

Can I seriously not just add an unnamed socket to my board and have me wire up the connections manually? Do I really have to create a whole new part with every pin predefined? That would be insane, and incredibly frustrating for a newcomer like myself. I could see myself end up using hours figuring that out image

 

The specific part I'm trying to add is PLCC-68 SMTL-TT. It's for a Motorola 68000 on a Neo Geo MV-1C.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 10 years ago

    Hi Martin,

     

    You do need to create a part (if one doesn't exist) to reflect what you want in the schematic, and then it will place the footprint in the board layout view. While your requirement is valid for very small circuits, it wouldn't scale to larger circuits without a high risk of error and is therefore a workflow that isn't supported in many CAD packages.

    Some early low-cost CAD packages allowed you to place and wire package footprints manually, and there are still some software packages which do this. I think Sprint-Layout supports the type of workflow you want to do.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 10 years ago

    Hi Martin,

     

    You do need to create a part (if one doesn't exist) to reflect what you want in the schematic, and then it will place the footprint in the board layout view. While your requirement is valid for very small circuits, it wouldn't scale to larger circuits without a high risk of error and is therefore a workflow that isn't supported in many CAD packages.

    Some early low-cost CAD packages allowed you to place and wire package footprints manually, and there are still some software packages which do this. I think Sprint-Layout supports the type of workflow you want to do.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • konsolkongen
    0 konsolkongen over 10 years ago in reply to shabaz

    Hi shabaz. Thank you for your reply. I do see the benefit in having the part properly defined for large runs, or parts you use regularly. For this one though it's a bit annoying as I don't ever plan on using it again image

     

    But at least I now know that this is the correct way, so there's no getting around it, as I would like to stick with Eagle. I have to figure out how to add a new part, and it will probably be handy down the line too.

     

    I have added the package? (the drawing from the smd-special library) to a new library, so I guess I need to figure out how to add the stuff that goes into the schematic view image