Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Trying to add PLCC68 socket from the smd-special.lbr
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1586 views
  • Users 0 members are here
  • eagle
  • socket
  • plcc
Related

Trying to add PLCC68 socket from the smd-special.lbr

konsolkongen
konsolkongen over 9 years ago

Hi. I'm new to Eagle. I know the very basics of how to use it, but I have some problems adding a part to my board. I wan't to add a PLCC68 socket, which is included in the smd-special library. I just want the empty socked and I can wire up all the connections manually.

 

However, the socket cannot be found when in schematics mode, where I would normally add it. I can only find it when in board design, and there I'm not allowed to add it. I get the error "Can't backannotate this operation. Please do this in the schematic!", which as I said is not possible because the part does not show up there.

 

Can I seriously not just add an unnamed socket to my board and have me wire up the connections manually? Do I really have to create a whole new part with every pin predefined? That would be insane, and incredibly frustrating for a newcomer like myself. I could see myself end up using hours figuring that out image

 

The specific part I'm trying to add is PLCC-68 SMTL-TT. It's for a Motorola 68000 on a Neo Geo MV-1C.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 09/20/2016 05:13 PM, Martin Larsen wrote:

    Hi. I'm new to Eagle. I know the very basics of how to use it, but I

    have some problems adding a part to my board. I wan't to add a PLCC68

    socket, which is included in the smd-special library. I just want the

    empty socked and I can wire up all the connections manually.

     

    This library contains mostly packages, not devices (except for some SMD

    DIP switches). There are no devices associated with the PLCC-68-SMTL-TT

    package in this library.

     

    However, the socket cannot be found when in schematics mode, where I

    would normally add it. I can only find it when in board design, and

    there I'm not allowed to add it. I get the error "Can't backannotate

    this operation. Please do this in the schematic!", which as I said is

    not possible because the part does not show up there.

     

    The schematic editor works with devices that contain symbols. To add a

    device to a schematic you need a complete device, which includes a

    symbol and zero or more packages.

     

    Can I seriously not just add an unnamed socket to my board and have

    me wire up the connections manually? Do I really have to create a

    whole new part with every pin predefined? That would be insane, and

    incredibly frustrating for a newcomer like myself. I could see myself

    end up using hours figuring that out image

     

    Seriously, no. The proper way to do this is to create a symbol for the

    device, then create a device using your symbol and the appropriate

    package. If you want to you can copy the package from the supplied

    library, but if you're smart you'll verify that the package has the

    characteristics you really want and not blindly trust it.

     

    Your symbol doesn't have to be a work of art. It can be just a box with

    a bunch of numbered pins. Most people will tell you that it'll be more

    useful if you add useful information about the device, though.

     

    This really isn't hard to do, and the docs include a tutorial for doing it.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 09/20/2016 05:13 PM, Martin Larsen wrote:

    Hi. I'm new to Eagle. I know the very basics of how to use it, but I

    have some problems adding a part to my board. I wan't to add a PLCC68

    socket, which is included in the smd-special library. I just want the

    empty socked and I can wire up all the connections manually.

     

    This library contains mostly packages, not devices (except for some SMD

    DIP switches). There are no devices associated with the PLCC-68-SMTL-TT

    package in this library.

     

    However, the socket cannot be found when in schematics mode, where I

    would normally add it. I can only find it when in board design, and

    there I'm not allowed to add it. I get the error "Can't backannotate

    this operation. Please do this in the schematic!", which as I said is

    not possible because the part does not show up there.

     

    The schematic editor works with devices that contain symbols. To add a

    device to a schematic you need a complete device, which includes a

    symbol and zero or more packages.

     

    Can I seriously not just add an unnamed socket to my board and have

    me wire up the connections manually? Do I really have to create a

    whole new part with every pin predefined? That would be insane, and

    incredibly frustrating for a newcomer like myself. I could see myself

    end up using hours figuring that out image

     

    Seriously, no. The proper way to do this is to create a symbol for the

    device, then create a device using your symbol and the appropriate

    package. If you want to you can copy the package from the supplied

    library, but if you're smart you'll verify that the package has the

    characteristics you really want and not blindly trust it.

     

    Your symbol doesn't have to be a work of art. It can be just a box with

    a bunch of numbered pins. Most people will tell you that it'll be more

    useful if you add useful information about the device, though.

     

    This really isn't hard to do, and the docs include a tutorial for doing it.