Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Best way to upgrade
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 13 answers
  • Subscribers 190 subscribers
  • Views 4406 views
  • Users 0 members are here
Related

Best way to upgrade

jsantosrico
jsantosrico over 9 years ago

Hi,

 

The default behaviour of Eagle is to keep old versions of eagle when you update. Is not really a problem, as it is not hughe program, but it's a tad annoying when I click an old link pointing to an old version or I double click on a file and it opens in the old version because the file association has not updated. Why is this the default behaviour? I also noted that in my projects there is a file called Eagle.epf, which lists the libraries in use in my project, and the default libraries still point to old versions of them, as in for example:

 

....

UsedLibrary="C:/EAGLE-7.6.0/lbr/19inch.lbr"

UsedLibrary="C:/EAGLE-7.6.0/lbr/40xx.lbr"

UsedLibrary="C:/EAGLE-7.6.0/lbr/41xx.lbr"

UsedLibrary="C:/EAGLE-7.6.0/lbr/45xx.lbr"

....

 

Do I have to check all my projects every time I upgrade and update to the new paths? Is that the way this is intended to be? I was wondering if there is a less cumbersome way to update.

 

Thanks for taking the time to check my problem.

 

regards,

 

Joel

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 7 years ago

    Eagle? Is it still in use?image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 7 years ago in reply to clem57

    Real numbers are hard to come by. The last numbers I saw indicate Eagle has a small market share by revenue numbers, but it has orders of magnitude more users than big names like Mentor, Cadence and Altium. (because of its decent free package) Presumably AutoCad is trying to convert all those users into paying customers with novel licensing schemes. Unfortunately they risk losing some of the user base in the process.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 7 years ago in reply to dougw

    Around 2003 I spent a few months designing with the free version of Eagle before taking the plunge and buying the full version. I had to upgrade when they changed the library structure. I still design a lot of circuits and boards with Eagle using my old version, but have not used any of the versions introduced after they moved to a subscription based license.

    Out of all the new users that start with a free CAD tool, only a fixed small percentage will ever switch to a paid version. Autodesk may increase this percentage somewhat by keeping the initial cost low, but it is important that a decent free version is available, otherwise new users will choose a different tool and follow a different upgrade path. The company with the best free tool is going to have a larger base from which to gain paying converts.

    Unfortunately, the subscription method doesn't appeal to me and I will likely never use it, even though newer versions of Eagle have some nice new features.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 7 years ago in reply to dougw

    Around 2003 I spent a few months designing with the free version of Eagle before taking the plunge and buying the full version. I had to upgrade when they changed the library structure. I still design a lot of circuits and boards with Eagle using my old version, but have not used any of the versions introduced after they moved to a subscription based license.

    Out of all the new users that start with a free CAD tool, only a fixed small percentage will ever switch to a paid version. Autodesk may increase this percentage somewhat by keeping the initial cost low, but it is important that a decent free version is available, otherwise new users will choose a different tool and follow a different upgrade path. The company with the best free tool is going to have a larger base from which to gain paying converts.

    Unfortunately, the subscription method doesn't appeal to me and I will likely never use it, even though newer versions of Eagle have some nice new features.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer