EAGLE User Support (English) Best way to upgrade
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
  • State Suggested Answer
  • Replies 25 replies
  • Answers 13 answers
  • Subscribers 182 subscribers
  • Views 3691 views
  • Users 0 members are here
Related

Best way to upgrade

jsantosrico
jsantosrico over 9 years ago

Hi,

 

The default behaviour of Eagle is to keep old versions of eagle when you update. Is not really a problem, as it is not hughe program, but it's a tad annoying when I click an old link pointing to an old version or I double click on a file and it opens in the old version because the file association has not updated. Why is this the default behaviour? I also noted that in my projects there is a file called Eagle.epf, which lists the libraries in use in my project, and the default libraries still point to old versions of them, as in for example:

 

....

UsedLibrary="C:/EAGLE-7.6.0/lbr/19inch.lbr"

UsedLibrary="C:/EAGLE-7.6.0/lbr/40xx.lbr"

UsedLibrary="C:/EAGLE-7.6.0/lbr/41xx.lbr"

UsedLibrary="C:/EAGLE-7.6.0/lbr/45xx.lbr"

....

 

Do I have to check all my projects every time I upgrade and update to the new paths? Is that the way this is intended to be? I was wondering if there is a less cumbersome way to update.

 

Thanks for taking the time to check my problem.

 

regards,

 

Joel

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 6 years ago in reply to geralds +5 suggested
    geralds wrote: AD was or is extremely expensive with its software tools every time. ... Then you need a full version. Well, then the price shoots up like a rocket. I don't think EAGLE is particularly expensive…
  • shabaz
    shabaz over 6 years ago in reply to geralds +5 suggested
    I really like EAGLE, and tried hard to see if I could work with the pricing model, since I wanted the engineers to get paid well. But, from a perception perspective alone, the model is quite bad for hobbyists…
  • geralds
    geralds over 6 years ago in reply to dougw +3 suggested
    Yes, it seems so. The licensing scheme is a blocking wall for many old-Eagle user. AD was or is extremely expensive with its software tools every time. With the free version of Eagle you can do everything…
  • clem57
    0 clem57 over 6 years ago

    Eagle? Is it still in use?image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 6 years ago in reply to clem57

    clem57  wrote:

     

    Eagle? Is it still in use?image

     

    Yes and it's going from strength to strength, have you looked at the features added in the more recent versions?

     

    But why are you dredging up posts from years ago? Trying to level up are we? image image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 6 years ago in reply to rachaelp

    I was not being snarky, but really wondered..

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • geralds
    0 geralds over 6 years ago in reply to clem57

    The recent version is 9.5.0. This version has a lot of new functions as well.

    https://www.autodesk.com/products/eagle/blog/whats-new-in-autodesk-eagle-9-5/

     

    You can download it here:

    https://www.autodesk.com/products/eagle/free-download

     

    Gerald

    ---

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 6 years ago in reply to clem57

    Am 23.08.2019 um 19:30 schrieb BB-Sphere (Clem):

    Eagle? Is it still in use?:p

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/279926

     

     

    I've seen what you have posted before...

    If you have nothing else to say you better shut up.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 6 years ago

    Am 13.10.2016 um 15:55 schrieb Joel Santos Rico:

    Hi,

     

    The default behaviour of Eagle is to keep old versions of eagle when you update. Is not really a problem, as it is not hughe program, but it's a tad annoying when I click an old link pointing to an old version or I double click on a file and it opens in the old version because the file association has not updated. Why is this the default behaviour? I also noted that in my projects there is a file called Eagle.epf, which lists the libraries in use in my project, and the default libraries still point to old versions of them, as in for example:

     

    ...

    UsedLibrary="C:/EAGLE-7.6.0/lbr/19inch.lbr"

    UsedLibrary="C:/EAGLE-7.6.0/lbr/40xx.lbr"

    UsedLibrary="C:/EAGLE-7.6.0/lbr/41xx.lbr"

    UsedLibrary="C:/EAGLE-7.6.0/lbr/45xx.lbr"

    ...

     

    Do I have to check all my projects every time I upgrade and update to the new paths? Is that the way this is intended to be? I was wondering if there is a less cumbersome way to update.

     

    Thanks for taking the time to check my problem.

     

    regards,

     

    Joel

     

     

    Unfortunately you didn't mention your version of eagle nor your OS.

    Talking of win. There is an U-parameter that one can use to point to the

    eagle.exe file, i.e.

    E:EAGLE-5.12.0\bin\eagle.exe -U E:\Eagle-5.12.0\eaglerc-512.usr

    F:\EAGLE-6.6.0\bin\eagle.exe -U F:\Eagle-6.6.0\eaglerc-660.usr

     

    The file can have any name. I put them into the correspondent eagle

    version and name it i.e. "eaglerc-660.usr" instead of the original

    "eaglerc.usr" which is the name normally in EVERY eagle version (and

    causes problems).

    First part is the pointer to "eagle.exe" which is located in sub

    directory "bin", second part is the location of xxx.usr, in my case in

    the eagle main directory.

     

    I don't use the AD versions but think that this parameter still exist.

    Check documentation.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 6 years ago in reply to geralds

    Thanks Gerald. You answered my question.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 6 years ago in reply to autodeskguest

    On 31/08/2019 08:35, Joern Paschedag wrote:

     

    I don't use the AD versions but think that this parameter still exist.

    Check documentation.

    Yes, it still exists, and is very useful for having V9, V8, V7 and V5

    all available on the same PC, in case I need to work on an old design

    and don't want to convert it.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 6 years ago in reply to autodeskguest

    autodeskguest  wrote:

     

    I don't use the AD versions

     

    It's a shame more of the long time users of the original EAGLE like yourself aren't using the newer AD versions, your experience and support on the main AD forums would be very valuable and I'm sure if you could look past the licensing (which I assume is your reason for not using it), it's actually really really good now. It's like old EAGLE on steroids, the last few releases in particular have been big jumps up in functionality.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago in reply to clem57

    Real numbers are hard to come by. The last numbers I saw indicate Eagle has a small market share by revenue numbers, but it has orders of magnitude more users than big names like Mentor, Cadence and Altium. (because of its decent free package) Presumably AutoCad is trying to convert all those users into paying customers with novel licensing schemes. Unfortunately they risk losing some of the user base in the process.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
>