EAGLE User Support (English) Best way to upgrade
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
  • State Suggested Answer
  • Replies 25 replies
  • Answers 13 answers
  • Subscribers 181 subscribers
  • Views 3500 views
  • Users 0 members are here
Related

Best way to upgrade

jsantosrico
jsantosrico over 9 years ago

Hi,

 

The default behaviour of Eagle is to keep old versions of eagle when you update. Is not really a problem, as it is not hughe program, but it's a tad annoying when I click an old link pointing to an old version or I double click on a file and it opens in the old version because the file association has not updated. Why is this the default behaviour? I also noted that in my projects there is a file called Eagle.epf, which lists the libraries in use in my project, and the default libraries still point to old versions of them, as in for example:

 

....

UsedLibrary="C:/EAGLE-7.6.0/lbr/19inch.lbr"

UsedLibrary="C:/EAGLE-7.6.0/lbr/40xx.lbr"

UsedLibrary="C:/EAGLE-7.6.0/lbr/41xx.lbr"

UsedLibrary="C:/EAGLE-7.6.0/lbr/45xx.lbr"

....

 

Do I have to check all my projects every time I upgrade and update to the new paths? Is that the way this is intended to be? I was wondering if there is a less cumbersome way to update.

 

Thanks for taking the time to check my problem.

 

regards,

 

Joel

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 6 years ago in reply to geralds +5 suggested
    geralds wrote: AD was or is extremely expensive with its software tools every time. ... Then you need a full version. Well, then the price shoots up like a rocket. I don't think EAGLE is particularly expensive…
  • shabaz
    shabaz over 6 years ago in reply to geralds +5 suggested
    I really like EAGLE, and tried hard to see if I could work with the pricing model, since I wanted the engineers to get paid well. But, from a perception perspective alone, the model is quite bad for hobbyists…
  • geralds
    geralds over 6 years ago in reply to dougw +3 suggested
    Yes, it seems so. The licensing scheme is a blocking wall for many old-Eagle user. AD was or is extremely expensive with its software tools every time. With the free version of Eagle you can do everything…
  • geralds
    0 geralds over 6 years ago in reply to dougw

    Yes, it seems so.

    The licensing scheme is a blocking wall for many old-Eagle user.

    AD was or is extremely expensive with its software tools every time.

     

    With the free version of Eagle you can do everything with its functions which you can do with the premium version, but you have no adequate routing space on the PCB (80x100mm, with 2 signal layer).

    So, if you like mounting a "large" device, e.g. a 100 pin SMD IC with its components, the placing space will be overflow very quickly.

    Then you need a full version. Well, then the price shoots up like a rocket.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 6 years ago in reply to geralds

    geralds  wrote:

     

    AD was or is extremely expensive with its software tools every time.

     

    ...

     

    Then you need a full version. Well, then the price shoots up like a rocket.

     

    I don't think EAGLE is particularly expensive, If you do commercial work and want the standard version it's £114/year, if you need the premium version it's £600/year. For hobby work then it's possibly a bit steep for the premium version, but it was never free for the equivalents of these pre-subscription either. Compare the premium version to the likes of Mentor and Altium and you can get many seats for the cost of just one of the market leaders. Yes it doesn't do quite everything they do, but it's getting a lot closer. I understand why some people don't like the subscription but nobody can accuse Autodesk of creaming the profits from EAGLE and not putting the effort in to update the software, compare 9.5 to 7.6 (pre Autodesk) and it's night and day in terms of capability.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • geralds
    0 geralds over 6 years ago in reply to rachaelp

    Hi Rachael, rachaelp

    Yes, that's right and true.

    Many smaller companies may not use such CAD programs every day. So a subscription scheme, especially if you need several tools "at the same time", can quickly become expensive.Smaller companies may also have other offerings or services, so working alone with CAD programs can be costly rather than money-making.

    For me e.g., I also offer building of prototype modules, or programming of Microcontroller controlled modules. Then every day of the year is valuable considering Eagle-CAD.

     

    Yes, we remember what discussions we had here at E14 in the Autodesk Community back then.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to geralds

    I really like EAGLE, and tried hard to see if I could work with the pricing model, since I wanted the engineers to get paid well.

     

    But, from a perception perspective alone, the model is quite bad for hobbyists : ( I really wanted a decent pricing model for 4-layer hobbyists (such as those who have grown up with EAGLE perhaps).

     

    Having to subscribe and unsubscribe for 4-layer is going to always be seen as cost-inefficient (and inconvenient having to remember switching subscriptions off) because hobbyists are unlikely to make full use of it for an entire month. So that could leave hobbyists feeling they are not getting value for money.

     

    They are basically falling in a gap where they get considered and fully charged as commercial users, which they're not : (

     

    I've no issue paying for other software including modern rental software, and including older licensing models like upgrades,

    but prefer those where there is less inconvenience, and fairer for hobbyists.

     

    Some RF software manufacturer charges $30 per year, so I pay that, it seems fair for hobbyists.

    $15 per month for EAGLE seems unfair considering that's not a hobbyist amount, that's for commercial. I fully understand they need to draw the line somwhere, and unfortunately for some of us, the line is in the wrong place, and it is what it is : ( For this reason, although I still keep up-to-date with what EAGLE features there are, I feel I cannot upgrade for hobbyist use any more : (

     

    Matlab makes on average £30-40 a year from me, since I don't upgrade every year, I'll skip some years. That's £30-40 more than they otherwise would make, since I'd move off to (say) Gnu Octave if the cost was much higher.

     

    Same with other Adobe stuff like Lightroom, I preferred upgrading every few years when it was convenient for me, and not paying for every release, but I cannot do that now. So I've moved off that, to Capture One, even though it costs more initially, I'll average less per year until I eventually upgrade to the latest version.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago in reply to dougw

    Around 2003 I spent a few months designing with the free version of Eagle before taking the plunge and buying the full version. I had to upgrade when they changed the library structure. I still design a lot of circuits and boards with Eagle using my old version, but have not used any of the versions introduced after they moved to a subscription based license.

    Out of all the new users that start with a free CAD tool, only a fixed small percentage will ever switch to a paid version. Autodesk may increase this percentage somewhat by keeping the initial cost low, but it is important that a decent free version is available, otherwise new users will choose a different tool and follow a different upgrade path. The company with the best free tool is going to have a larger base from which to gain paying converts.

    Unfortunately, the subscription method doesn't appeal to me and I will likely never use it, even though newer versions of Eagle have some nice new features.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 6 years ago in reply to autodeskguest

    Am 31.08.2019 um 11:44 schrieb Rob Pearce:

    On 31/08/2019 08:35, Joern Paschedag wrote:

     

    I don't use the AD versions but think that this parameter still exist.

    Check documentation.

    Yes, it still exists, and is very useful for having V9, V8, V7 and V5

    all available on the same PC, in case I need to work on an old design

    and don't want to convert it.

     

     

    That is exactly the reason why I keep old versions image

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 6 years ago in reply to rachaelp

    Am 31.08.2019 um 15:33 schrieb rachaelp:

      wrote:

     

    I don't use the AD versions

     

    It's a shame more of the long time users of the original EAGLE like yourself aren't using the newer AD versions, your experience and support on the main AD forums would be very valuable and I'm sure if you could look past the licensing (which I assume is your reason for not using it), it's actually really really good now. It's like EAGLE on steroids, the last few releases in particular have been big jumps up in functionality.

     

    Best Regards,

     

    Rachael

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/280300

     

     

    A shame is AD's attitude...

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 6 years ago in reply to autodeskguest

    On 9/1/19 03:27, Joern Paschedag wrote:

    Am 31.08.2019 um 15:33 schrieb rachaelp:

       wrote:

     

    I don't use the AD versions

     

    It's a shame more of the long time users of the original EAGLE like

    yourself aren't using the newer AD versions

    ...

     

    A shame is AD's attitude...

     

    Good afternoon, Rachael,

     

    Like Joern, myself, and others, you're a long time user of Eagle.  I

    recall that you were vocal regarding AD's licensing policy.  I was as

    well.  I believe that we engaged each other in a... not heated... but an

    "energetic" debate, which I found quite enjoyable.  We both were able to

    clearly convey our respective policies.  While I understand your view on

    this, I have not adopted it as my own.

     

    I wouldn't call it a shame that long time users such as myself aren't

    using the newer AD versions of Eagle.  We're probably missing out on

    some new features and such, but we're getting along with the pre-8.0

    versions.  My company hasn't had a compelling need for anything more

    feature rich that 7.7.  Instead, it's more of a disappointment that AD

    is not willing to provide an off-line or perpetual license.

     

    The true shame lies with AD when, despite their promise, they absolutely

    refused to accommodate users needing a perpetual license.  I mean, they

    weren't even will to enter into one-on-one negotiations.  And /that/ is

    to what Jeorn eluded.

     

    Just for completeness, Eagle is not the only AutoDesk product I can't use.

     

    For now, I'll continue using Eagle 7.7.  When I need new features, I'll

    look elsewhere... but not to AutoDesk, at least not until they willing

    to negotiate in good faith.

     

    Rachel, It is sincerely enjoyable to exchange ideas with you.  I look

    forward to the next time we can engage.

     

    Enjoy,

        - Chuck

     

     

     

    Attachments:
    3051.att1.html.zip
    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 6 years ago in reply to dukepro

    Hi Chuck,

     

    It's great to hear from you and thank you for replying on this.

     

    dukepro  wrote:

     

    I wouldn't call it a shame that long time users such as myself aren't using the newer AD versions of Eagle. 

     

    I guess what I should have said was I personally find it a shame that the situation has lead to a lot of the long time EAGLE users to not being involved in how EAGLE has progressed, and not being on those forums. I always found your and many others insights invaluable. So it's me personally wishing the situation was different and you guys would be involved in the new EAGLE forums again. I really do understand and respect your position on this but still hope that some day something can be done to improve this situation.

     

    I don't know if you have even looked casually at the more recent changes, but for me the productivity increase over what I can do in 7.7 for the boards I do is massive and at least some of the early accusations levelled at AD that they were just in it to fleece people for the subscription money have been proven false.

     

    AD corporate licensing policies aside, it seems to be a really genuinely enthusiastic bunch of engineers working on bringing new features to EAGLE and it's a shame for them too that no matter how hard they work and how much they add to the product, there are a large portion of the potential user base who are not going to use what they are producing.

     

    dukepro  wrote:

     

    Rachel, It is sincerely enjoyable to exchange ideas with you.  I look

    forward to the next time we can engage.

     

    Likewise, hopefully our paths will cross again in the not too distant future.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • geralds
    0 geralds over 6 years ago in reply to dukepro

    Basically, I think like you. But Autodesk does not care how many cope. That was so every time, with all their products they sell.

    "If you like that, or need that - then pay that!"

    I recall too what we discussed here.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>