EAGLE User Support (English) Best way to upgrade
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
  • State Suggested Answer
  • Replies 25 replies
  • Answers 13 answers
  • Subscribers 181 subscribers
  • Views 3503 views
  • Users 0 members are here
Related

Best way to upgrade

jsantosrico
jsantosrico over 9 years ago

Hi,

 

The default behaviour of Eagle is to keep old versions of eagle when you update. Is not really a problem, as it is not hughe program, but it's a tad annoying when I click an old link pointing to an old version or I double click on a file and it opens in the old version because the file association has not updated. Why is this the default behaviour? I also noted that in my projects there is a file called Eagle.epf, which lists the libraries in use in my project, and the default libraries still point to old versions of them, as in for example:

 

....

UsedLibrary="C:/EAGLE-7.6.0/lbr/19inch.lbr"

UsedLibrary="C:/EAGLE-7.6.0/lbr/40xx.lbr"

UsedLibrary="C:/EAGLE-7.6.0/lbr/41xx.lbr"

UsedLibrary="C:/EAGLE-7.6.0/lbr/45xx.lbr"

....

 

Do I have to check all my projects every time I upgrade and update to the new paths? Is that the way this is intended to be? I was wondering if there is a less cumbersome way to update.

 

Thanks for taking the time to check my problem.

 

regards,

 

Joel

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 6 years ago in reply to geralds +5 suggested
    geralds wrote: AD was or is extremely expensive with its software tools every time. ... Then you need a full version. Well, then the price shoots up like a rocket. I don't think EAGLE is particularly expensive…
  • shabaz
    shabaz over 6 years ago in reply to geralds +5 suggested
    I really like EAGLE, and tried hard to see if I could work with the pricing model, since I wanted the engineers to get paid well. But, from a perception perspective alone, the model is quite bad for hobbyists…
  • geralds
    geralds over 6 years ago in reply to dougw +3 suggested
    Yes, it seems so. The licensing scheme is a blocking wall for many old-Eagle user. AD was or is extremely expensive with its software tools every time. With the free version of Eagle you can do everything…
  • autodeskguest
    0 autodeskguest over 6 years ago in reply to rachaelp

    Am 03.09.2019 um 17:58 schrieb rachaelp:

    Hi Chuck,

     

    It's great to hear from you and thank you for replying on this.

     

      wrote:

     

    I wouldn't call it a shame that long time users such as myself aren't using the newer AD versions of Eagle.

     

    I guess what I should have said was I personally find it a shame that the situation has lead to a lot of the long time EAGLE users to not being involved in how EAGLE has progressed, and not being on those forums. I always found your and many others insights invaluable. So it's me personally wishing the situation was different and you guys would be involved in the new EAGLE forums again. I really do understand and respect your position on this but still hope that some day something can be done to improve this situation.

     

     

    Hi Rachael,

    I don't feel bothered image

     

    On the other hand I don't consider you as a long time user (around 2016

    I guess)?

     

    And I shall not start again a discussion about the old stuff.

    But what you don't know is during that time after some long open

    discussions some others and I  got private offers from AD about licensing.

    Imho behind the back of all the other users.

    Same thing is  AD's "condition of use".

    Have you ever read through the whole of it? Especially I "like" position

    9 and 11.1.

    THAT certainly takes time  (that is made so to lull one in, put one asleep)

    but I always do read through the whole thing and those conditions are

    not acceptable for me.

    Imho it shows the character of AD and I don't like it.

     

    I don't know if you have even looked casually at the more recent changes, but for me the productivity increase over what I can do in 7.7 for the boards I do is massive and at least some of the early accusations levelled at AD that they were just in it to fleece people for the subscription money have been proven false.

     

    AD corporate licensing policies aside, it seems to be a really genuinely enthusiastic bunch of engineers working on bringing new features to EAGLE and it's a shame for them too that no matter how hard they work and how much they add to the product, there are a large portion of the potential user base who are not going to use what they are producing.

     

     

    Well I see that a little different. What I have seen in the the update

    list is that most of the new updates are repairs of a few new things.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 6 years ago in reply to autodeskguest

    Hi Joern,

     

    autodeskguest  wrote:

     

    Hi Rachael,

    I don't feel bothered image

     

    On the other hand I don't consider you as a long time user (around 2016

    I guess)?

     

    I've been using EAGLE professionally since early 2015 but on and off for personal projects way before that, but I was only active on the forums from 2015. Prior to using EAGLE for my main work I used Mentor Graphics and Cadence products for many years so I know what higher end tools are like and what the features add to the workflow.

     

    autodeskguest  wrote:

     

    Same thing is  AD's "condition of use".

    Have you ever read through the whole of it? Especially I "like" position

    9 and 11.1.

     

    Well I can certainly understand that the wording of these may cause some concern....

     

    autodeskguest  wrote:

     

    Well I see that a little different. What I have seen in the the update list is that most of the new updates are repairs of a few new things.

     

    Certainly a lot of what is listed in the release notes is related to enhancement/fixes to existing features but having read through it now the release notes aren't always doing a good job of highlighting all the new features properly. There is a lot more than is immediately obvious from a scan through the release notes. Here is a list of the things I can think of:

     

    • Shared Managed Libraries
    • Design Manager in Schematic
    • Persistent Groups
    • Re-Route Command
    • New Routing Engine with new Bus Routing and enhanced Diff Pair Routing
    • Selection Filter and Object Inspector
    • Assign 3D models in Sch/Brd
    • Quickroute Fanout
    • Preserve Angles Move in Board
    • Digital/Mixed Simulation
    • Design Manager in Board
    • New Bus UI functionality in the schematic
    • New CAM Processor
    • Analog SPICE Simulation
    • Routing enhanced with Object Avoidance, Loop Removal, Push & Shove, Etc
    • Live DRC
    • Fusion 360 Integration

     

    There's probably a lot more I have forgotten too, not that I expect you care at this point image

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 6 years ago in reply to rachaelp

    Am 04.09.2019 um 13:57 schrieb rachaelp:

    Hi Joern,

     

      wrote:

     

    Hi Rachael,

    I don't feel bothered

     

    On the other hand I don't consider you as a long time user (around 2016

    I guess)?

     

    I've been using EAGLE professionally since early 2015 but on and off for personal projects way before that, but I was only active on the forums from 2015. Prior to using EAGLE for my main work I used Mentor Graphics and Cadence products for many years so I know what higher end tools are like and what the features add to the workflow.

     

     

    SNIP

     

    I see image

    I started with Orcad...

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 6 years ago in reply to autodeskguest

    On 9/4/19 11:47, Joern Paschedag wrote:

    Am 04.09.2019 um 13:57 schrieb rachaelp:

    Hi Joern,

     

       wrote:

      Hi Rachael,

    I don't feel bothered

     

    On the other hand I don't consider you as a long time user (around 2016

    I guess)?

     

    I've been using EAGLE professionally since early 2015 but on and off

    for personal projects way before that, but I was only active on the

    forums from 2015. Prior to using EAGLE for my main work I used Mentor

    Graphics and Cadence products for many years so I know what higher

    end tools are like and what the features add to the workflow.

     

     

    SNIP

     

    I see image

    I started with Orcad...

     

    Yeah.. that's pretty close to where I started.

     

    Orcad schematic and Tango PCB in the early-mid 80's.

     

    I'm not entirely sure when I cut over to Eagle.  I do know it was

    sometime in version 4.

     

    Enjoy,

        - Chuck

     

    Attachments:
    7455.att1.html.zip
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 6 years ago in reply to dukepro

    Am 04.09.2019 um 23:15 schrieb Chuck Huber:

    On 9/4/19 11:47, Joern Paschedag wrote:

    Am 04.09.2019 um 13:57 schrieb rachaelp:

    Hi Joern,

     

       wrote:

      Hi Rachael,

    I don't feel bothered

     

    On the other hand I don't consider you as a long time user (around 2016

    I guess)?

     

    I've been using EAGLE professionally since early 2015 but on and off

    for personal projects way before that, but I was only active on the

    forums from 2015. Prior to using EAGLE for my main work I used Mentor

    Graphics and Cadence products for many years so I know what higher

    end tools are like and what the features add to the workflow.

     

     

    SNIP

     

    I see image

    I started with Orcad...

     

    Yeah.. that's pretty close to where I started.

     

    Orcad schematic and Tango PCB in the early-mid 80's.

     

    I'm not entirely sure when I cut over to Eagle.  I do know it was

    sometime in version 4.

     

    Enjoy,

        - Chuck

     

    I just checked, I started with eagle 2.6, still have the Cadsoft folder  image

    with 5 1/4" diskettes and no drive for them image

    The reason was actually that I had to construct plenty devices with

    European symbols in orcad.

    When eagle came out we had both the US- and EU-Symbols and we even could

    convert the orcad files to eagle.

    Unfortunately there was no hierarchical design in eagle but was no so

    important at that time.

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<