Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Drill File Generation
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 811 views
  • Users 0 members are here
  • drill file
  • drd
  • cam
  • excellon
Related

Drill File Generation

antifluxion
antifluxion over 9 years ago

I am using Eagle 6.6.0 with a professional license and I am running into an interesting problem in the drill file generation. The 'run drillcfg' command runs without any problems, however, there is a problem in running the excellon job: While the .dri file is created correctly, there seems to be a problem in generating the .drd file. Instead of a single .drd file, there are two files that are generated with the extensions *.drd.0116 and *.drd.0215. Any ideas what this might mean?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    Nathan Szanto wrote on Mon, 31 October 2016 20:09

    I am using Eagle 6.6.0 with a professional license and I am running

    into an interesting problem in the drill file generation. The 'run

    drillcfg' command runs without any problems, however, there is a problem

    in running the excellon job: While the .dri file is created correctly,

    there seems to be a problem in generating the .drd file. Instead of a

    single .drd file, there are two files that are generated with the

    extensions *.drd.0116 and *.drd.0215. Any ideas what this might mean?

     

     

    Two .drd files means there are two types of vias in the design.  EAGLE can

    do both blind and buried vias but those are only needed for quiet complex

    boards.  They are defined in the Layer setup window that is found by

    running the DRC command and clicking on the DRC tab.  The instructions

    there are a bit obtuse but it is complete and correct.

     

    The via types are shown visually.  If you only want "normal" vias that go

    from the top layer to the bottom layer then you should just see one

    instance of a via.  If you inadvertently enabled blind or buried vias

    you'll see another via that shows the subset of layers that they are

    allowed to encompass.  You'll have to change the setup string to allow only

    one type of vias and then change all the vias in your design to be the

    default 1-16 type.

     

    Hope that helps,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Order your EAGLE license from Stratford Digital at

    http://www.eaglelicenses.com

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 9 years ago

    Nathan Szanto wrote on Mon, 31 October 2016 20:09

    I am using Eagle 6.6.0 with a professional license and I am running

    into an interesting problem in the drill file generation. The 'run

    drillcfg' command runs without any problems, however, there is a problem

    in running the excellon job: While the .dri file is created correctly,

    there seems to be a problem in generating the .drd file. Instead of a

    single .drd file, there are two files that are generated with the

    extensions *.drd.0116 and *.drd.0215. Any ideas what this might mean?

     

     

    Two .drd files means there are two types of vias in the design.  EAGLE can

    do both blind and buried vias but those are only needed for quiet complex

    boards.  They are defined in the Layer setup window that is found by

    running the DRC command and clicking on the DRC tab.  The instructions

    there are a bit obtuse but it is complete and correct.

     

    The via types are shown visually.  If you only want "normal" vias that go

    from the top layer to the bottom layer then you should just see one

    instance of a via.  If you inadvertently enabled blind or buried vias

    you'll see another via that shows the subset of layers that they are

    allowed to encompass.  You'll have to change the setup string to allow only

    one type of vias and then change all the vias in your design to be the

    default 1-16 type.

     

    Hope that helps,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Order your EAGLE license from Stratford Digital at

    http://www.eaglelicenses.com

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • antifluxion
    0 antifluxion over 9 years ago in reply to autodeskguest

    Yep, somehow we had a buried via in there and that's what was causing the problem. Thanks!