Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Change netname by wiring to copied Xref label
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 923 views
  • Users 0 members are here
  • xref
Related

Change netname by wiring to copied Xref label

steve@teradiode.com
steve@teradiode.com over 9 years ago

To make a connection between multiple pins for example without drawing a wired net, their netnames can be given the same name.  Once the first netname is assigned, each of the other names must be manually changed by editing the name.  It would be quicker and not require typing if the copy of a netname label as Xref could be directly wired to the other desired pins or connections.  Or just moved to the termination of an existing wire and the connection automatically made.  There probably should be a popup requesting confirmation of changing the netname, similar to what happens now if a netname if changed manually by typing and editing a new name.

 

Is this feasible or can it already be accomplished somehow?

 

Steve

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    Steve Parus wrote:

    To make a connection between multiple pins for example without drawing

    a wired net, their netnames can be given the same name.  Once the

    first netname is assigned, each of the other names must be manually

    changed by editing the name.  It would be quicker and not require

    typing if the copy of a netname label as Xref could be directly wired

    to the other desired pins or connections.  Or just moved to the

    termination of an existing wire and the connection automatically

    made.  There probably should be a popup requesting confirmation of

    changing the netname, similar to what happens now if a netname if

    changed manually by typing and editing a new name.

     

    1) draw the first net stub and attach the label.

    2) group the label and the end of the net stub it is connected to

    3) copy & paste as needed.

     

    the duplicates keep the net name and can be used to start other net

    segments.

     

    You can do this even for multiple nets at once.

     

     

    Be aware that placing the free end of such a copy on a pin won't

    connect.

    You will need to pick up the part and drop it in place to make the

    connection. But no need to do that for each single net, you can do it

    once after you have placed all nets for that part.

     

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 9 years ago

    Steve Parus wrote:

    To make a connection between multiple pins for example without drawing

    a wired net, their netnames can be given the same name.  Once the

    first netname is assigned, each of the other names must be manually

    changed by editing the name.  It would be quicker and not require

    typing if the copy of a netname label as Xref could be directly wired

    to the other desired pins or connections.  Or just moved to the

    termination of an existing wire and the connection automatically

    made.  There probably should be a popup requesting confirmation of

    changing the netname, similar to what happens now if a netname if

    changed manually by typing and editing a new name.

     

    1) draw the first net stub and attach the label.

    2) group the label and the end of the net stub it is connected to

    3) copy & paste as needed.

     

    the duplicates keep the net name and can be used to start other net

    segments.

     

    You can do this even for multiple nets at once.

     

     

    Be aware that placing the free end of such a copy on a pin won't

    connect.

    You will need to pick up the part and drop it in place to make the

    connection. But no need to do that for each single net, you can do it

    once after you have placed all nets for that part.

     

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • steve@teradiode.com
    0 steve@teradiode.com over 9 years ago in reply to autodeskguest

    Thanks Lorenz.

     

    The trick is to have a net wire connected to the netname label Xref and then group and copy both.  If only the label is copied, then a line is drawn from it back to its origin net as it is moved around, indicating I suppose that it is associated/locked to that net..

    I too observe that if the grouped label and net wire stub is initially moved such that the end of the stub contacts a pin, that connection is not actually made.  That can be observed by moving the pin or its component-there is no connection.  But moving the pin back so it contacts the end of the stub does result in the connection being made.  Alternatively, the initial placement can be made without contacting the pin and then the pin or its component moved so they do connect.

    The connectivity can be confirmed in the board layout.

     

    Steve