Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Change netname by wiring to copied Xref label
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 920 views
  • Users 0 members are here
  • xref
Related

Change netname by wiring to copied Xref label

steve@teradiode.com
steve@teradiode.com over 9 years ago

To make a connection between multiple pins for example without drawing a wired net, their netnames can be given the same name.  Once the first netname is assigned, each of the other names must be manually changed by editing the name.  It would be quicker and not require typing if the copy of a netname label as Xref could be directly wired to the other desired pins or connections.  Or just moved to the termination of an existing wire and the connection automatically made.  There probably should be a popup requesting confirmation of changing the netname, similar to what happens now if a netname if changed manually by typing and editing a new name.

 

Is this feasible or can it already be accomplished somehow?

 

Steve

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 2/12/2016 4:09 p.m., Steve Parus wrote:

    To make a connection between multiple pins for example without drawing a wired net, their netnames can be given the same name.  Once the first netname is assigned, each of the other names must be manually changed by editing the name.  It would be quicker and not require typing if the copy of a netname label as Xref could be directly wired to the other desired pins or connections.  Or just moved to the termination of an existing wire and the connection automatically made.  There probably should be a popup requesting confirmation of changing the netname, similar to what happens now if a netname if changed manually by typing and editing a new name.

     

    Is this feasible or can it already be accomplished somehow?

     

    Steve

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/210470

     

     

    Since a number of suggestions are appearing here (Not quite what the

    suggest forum is for) here is another approach.

     

    Enter in the command line, 'Net' and the name of the net you would like

    all over the place. Let's call it CLK

     

    NET CLK  and place an xref label directly.

     

    Now you have two command preloaded in the command line so use multiple

    up arrows to get the particular one you need.

     

    The nets are named with the desired name as you place them rather than

    going back and renaming them later.

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 2/12/2016 4:09 p.m., Steve Parus wrote:

    To make a connection between multiple pins for example without drawing a wired net, their netnames can be given the same name.  Once the first netname is assigned, each of the other names must be manually changed by editing the name.  It would be quicker and not require typing if the copy of a netname label as Xref could be directly wired to the other desired pins or connections.  Or just moved to the termination of an existing wire and the connection automatically made.  There probably should be a popup requesting confirmation of changing the netname, similar to what happens now if a netname if changed manually by typing and editing a new name.

     

    Is this feasible or can it already be accomplished somehow?

     

    Steve

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/210470

     

     

    Since a number of suggestions are appearing here (Not quite what the

    suggest forum is for) here is another approach.

     

    Enter in the command line, 'Net' and the name of the net you would like

    all over the place. Let's call it CLK

     

    NET CLK  and place an xref label directly.

     

    Now you have two command preloaded in the command line so use multiple

    up arrows to get the particular one you need.

     

    The nets are named with the desired name as you place them rather than

    going back and renaming them later.

     

    HTH

    Warren