Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 7.7 Access is denied
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 1 answer
  • Subscribers 192 subscribers
  • Views 2682 views
  • Users 0 members are here
  • eagle
  • eagle 7.7
Related

Eagle 7.7 Access is denied

ande
ande over 9 years ago

Hi,

When updated to 7.7 I can't save or open files. When opening it says: Locking of  (folder location) schem_2.sch failed. Access is denied.

And when closing Eagle 7.7 it says : Can't open (Folder  ) eaglerc.~~~   -> Permission denied.

 

I haven't change any folder options and older version are working just ok.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    Hello Antti,

     

    I hope you're doing well. What operating system are you using? If you

    are on Windows, did you allow EAGLE to install to the root of C like it

    wants to by default?

     

    The second symptom definitely looks like a permissions issue with the OS.

     

    For the first one, just disable file locking completely. If a .lck file

    was created then even if the feature is disabled EAGLE will still

    respect it. In that case you have to go delete the .lck file.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to autodeskguest

    Jorge Garcia wrote on Wed, 21 December 2016 17:32

    Hello Antti,

     

    For the first one, just disable file locking completely. If a .lck file

     

    was created then even if the feature is disabled EAGLE will still

    respect it. In that case you have to go delete the .lck file.

     

     

    Hi Jorge,

     

    I thought it was just file locking when I first looked at it but it's

    actually getting an access denied error when trying to create the lock

    which I think means this is related to the second issue too.

     

    Best Regards,

     

    Rachael

    --

    http://www.eaglecentral.ca :: The original and best browser access to CadSoft EAGLE support forums.  Supported by EAGLE licenses purchased through us :: http://www.eaglelicenses.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 9 years ago in reply to rachaelp

    On 12/21/2016 12:35 PM, Rachael wrote:

    Jorge Garcia wrote on Wed, 21 December 2016 17:32

    Hello Antti,

     

    For the first one, just disable file locking completely. If a .lck file

     

    was created then even if the feature is disabled EAGLE will still

    respect it. In that case you have to go delete the .lck file.

     

    Hi Jorge,

     

    I thought it was just file locking when I first looked at it but it's

    actually getting an access denied error when trying to create the lock

    which I think means this is related to the second issue too.

     

    Best Regards,

     

    Rachael

     

    I would like to hear the argument that resulted in a persistent lock

    from the use of a file as a boolean indicator.  The lockf(3) function is

    a POSIX standard function specifically designed to acquire, release, and

    test for locks.  And guess what... these locks are released by the

    kernel when the file is closed.  Since it's POSIX, it works on all three

    supported platforms and across all file systems (NFS, SMB, NTFS, FATxx,

    extx, jffs, and many others).

     

    See: https://linux.die.net/man/3/lockf

     

    So, why jump into all the problems associated with a persistent lock

    when such is best handled by a change management system (SCCS, RCS,

    Perforce, and many, many, others)?

     

    A question best posed to Jorge: by what process of ratiocination did the

    developers arrive at the conclusion that a using the presence or absence

    of a file is the best file locking method?  I'd like to hear their

    reason - maybe there's something I'm missing.

     

        - Chuck

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to dukepro

    A question best posed to Jorge: by what process of ratiocination did the

    developers arrive at the conclusion that a using the presence or absence

    of a file is the best file locking method?  I'd like to hear their

    reason - maybe there's something I'm missing.

     

        - Chuck

     

    Hi Chuck,

     

    That question is best left to the developers. Things are pretty hectic

    around here right now, but once things settle down a bit I'm going to

    put in an enhancement request on this, to either can it or reimplement it.

     

    When the best recommendation you can give about a feature is to not use

    it, there is a serious problem.

     

    Let me know if there's anything I can do for you.

     

    Best Regards,

    Jorge Garcia

     

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to rachaelp

    On 22/12/16 14:35, Rachael wrote:

    It's a very 1990's approach to solving

    the problem of multiple people sharing the same design files.

     

    Indeed, given that even MS Word seems to have stopped using that

    method since 2013 or so.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to rachaelp

    On 22/12/16 14:35, Rachael wrote:

    It's a very 1990's approach to solving

    the problem of multiple people sharing the same design files.

     

    Indeed, given that even MS Word seems to have stopped using that

    method since 2013 or so.