Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) dxf boardoutline
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 1917 views
  • Users 0 members are here
Related

dxf boardoutline

arny64
arny64 over 9 years ago

Hello i think i have posted in the right section this time, so i have drawn a dxf for my board outline in eagle not a terribly complex shape http://www.takachi-enclosure.com/data/c16-17/2016-043-48.pdf#6 .But when i import the dxf file into eagle using the import-dxf.ulp script i get some pretty rough edges on the arc and curves and some little tiny lines show up on the top copper layer.Iam more concerned of the tiny lines running across the top copper,but Is this just the limits of this script or is there anything i can do to round out all the rough edges and get rid of the lines thanks?

 

Iam using eagle 7.3 and have already tried in version 7.6 as well.

Here are what any of the arcs look like granted its not terrible but if i can make it better i will.My fab house said the line's wont be a problem but again if i can completely get rid of what is causing it i will.

 

The dxf is designed in Autodesk AutoCad 2015 in my original drawing of the dxf it would only draw straight lines none of the arc's or bend's in eagle would show up only straight lines,while saving the dxf in R12/LT2 dxf format any other dxf format would draw nothing in eagle.but since i completely redrawn the dxf i can save it in any dxf format and eagle will import but with the edges and lines.any input is appreciated thanks

image

  • Sign in to reply
  • Cancel
Parents
  • geralds
    0 geralds over 9 years ago

    Hi,

     

    I make the PCB complete in Eagle.

    You can draw this outline on the layer 20, Dimension; also for milling on the layer 46, Milling.

     

    It seems the PCB have a symmetrical shape.

    You can draw one half of the shape, then copy and mirror to the other side.

    Its very easy with drag and drop.

     

    Regards

    Gerald

    ---

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to geralds

    I think for the case the OP has given here you are right, it's simple enough to be drawn directly in EAGLE. But there are times when the board outline, holes, millings etc are a lot more complex with very accurate positioning required and the details are available already in AutoCAD from the mechanical engineers tools. It should be possible to reliably import DXF files into EAGLE to accurately replicate what the mechanical engineer designed. Fortunately now Autodesk own EAGLE they are responsible for both ends of the process so if something is broken here then it should be easier to get it fixed image

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • geralds
    0 geralds over 9 years ago in reply to rachaelp

    Absolutely agree.
    The point of the problem would be often that the mechanical engineers

    have tolerances in mm. But the PCB have it in µm.

    Often i have problems with rounding errors importing a DXF file.
    The next problem is that the DXF drawing is off-Grid in Eagle.

    Thinking about: "what can be so komplex that i cannot copy by drawing?"
    It's my philosophy.

    That's the point too that i often asked Cadsoft for an 3D viewer built in in Eagle.

     

    Autodesk is a very kompetent company which Autocad i use since the 1990is.

    I also hope that Eagle is growing up to a system like PCAD (this was my favorit in the old time of MSDOS), or Altium Designer.

    But many user then have the problem with jumping up of the expensive cost.

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • geralds
    0 geralds over 9 years ago in reply to rachaelp

    Absolutely agree.
    The point of the problem would be often that the mechanical engineers

    have tolerances in mm. But the PCB have it in µm.

    Often i have problems with rounding errors importing a DXF file.
    The next problem is that the DXF drawing is off-Grid in Eagle.

    Thinking about: "what can be so komplex that i cannot copy by drawing?"
    It's my philosophy.

    That's the point too that i often asked Cadsoft for an 3D viewer built in in Eagle.

     

    Autodesk is a very kompetent company which Autocad i use since the 1990is.

    I also hope that Eagle is growing up to a system like PCAD (this was my favorit in the old time of MSDOS), or Altium Designer.

    But many user then have the problem with jumping up of the expensive cost.

     

    Best Regards

    Gerald

    ---