EAGLE User Support (English) Eagle upgrade costs
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
  • State Suggested Answer
  • Replies 61 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 7954 views
  • Users 0 members are here
Related

Eagle upgrade costs

stevekale
stevekale over 9 years ago

I use the Make version of Eagle - something I may now come to regret versus starting with an open source package from the beginning.

 

I am not using the software for commercial use, rather for DIY audio electronics.  But I now need a board area greater than 16cm x 10cm. For my current project, I need about 20cm of length.  There appears to be nothing between Make and Ultimate for commercial use (with or without Autorouter which I do not use).

 

I wanted to check the upgrade cost yet when I enter my user license online to get an instant quote for upgrading  I merely get the  cost of buying a version from scratch - including an option to buy what I already have for what I have already paid.  Rather daft.

 

How to get the correct upgrade costs?  And am I the only one that would like to see a non-commercial offering with a larger board area at a more sensible price? (I will never need 4m x 4m board area, nor more than 4 signal layers.)  This is the sort of thing which forces people to learn KiCad or another competitor product.

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 9 years ago in reply to stevekale +2 suggested
    On 1/10/2017 7:47 AM, Steve Kale wrote: Hi. Thanks I will email them. It would be good if mattbergren can comment as the leap to Ultimate for DIY use is preventatively expensive. Regretfully I'm about…
  • e14candies
    e14candies over 9 years ago +1
    You can use some tricks and special editing commands to make a larger board if you really need to, however, it is much easier to upgrade Eagle to the size you need. Hopefully the new pricing/versions will…
  • rachaelp
    rachaelp over 9 years ago +1
    Looking on the cadsoft.io website this morning there is now a big splash screen saying the biggest release of EAGLE to date is coming soon. Judging by the snippets shown on that screen I have to say I…
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to autodeskguest

    On 03/23/2017 02:45 PM, warrenbrayshaw wrote:

    On 24/03/2017 6:40 a.m., Don Haselwood wrote:

    John,

     

    I'm trying to get my eagle version 4.13 running on Ubuntu 16.04 LTS on

    a 64b machine, but the window area with the schematic and board layout

    is blank, no matter what I do.  I did get the transparency issue

    resolved, but the inability to make anything appear in the work area

    window remains.  It appears to be a Ubuntu 16 issue as I do have an

    older machine running Ubuntu 14.04 and it is OK..  I wondered if you

    had that problem, and if so, what you did to fix it.   (I've tried all

    sorts of things I've found online having to do with the 32bit libs,

    but no success.)

     

    As far as upgrade goes--my paid version 4.13 is quite satisfactory for

    what I do (retired, hobbyist).  It produces what I want for the boards

    and the notion of no additional cost for eagle upgrades just doesn't

    offer anything.  (In my experience, software upgrades offer the hope

    of something better, but instead replace of old, known problems with

    new problems yet to be discovered.)  Kicad is attractive, but I can

    hit the right keys with my eagle 4.1 automatically without

    looking/thinking so continuing with eagle 4.1 (and not a later

    version!) is quite desirable.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/219285

     

     

    Hi Don

     

    Start by downloading the last point version of Eagle V4 (4.16r2) as your

    licence qualifies you for it.

     

    ftp://ftp.cadsoft.de/eagle/program/4.16r2/

     

    Then, I suspect there are some missing linux drivers that you will need

    to locate. This has been a problem from time to time.

     

    Others may be able to give you an exact answer.

     

    Failing that search the forum. I suspect E14 is not the place to do

    that. Search eagle central but let google do the heavy lifting when you

    have multpile works you wish to search for. e.g

     

    site:eaglecentral.ca  "linux drivers" "missing"

     

    HTH

    Warren

     

    I am running on a recent version of linux mint with xfce. Also on 4.x. I

    found the windows were transparent. I had to change the desktop setting

    (window mangager) to not use compositing. This fixed the transparent

    windows.

    With compositing enabled.

     

    Paul R. via newsgroup

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<