Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Add holes for through hole components
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 7 answers
  • Subscribers 190 subscribers
  • Views 8197 views
  • Users 0 members are here
Related

Add holes for through hole components

ardenne
ardenne over 9 years ago

Hi, I am new in the Eagle world and I am making a 2 layers custom board with Eagle. 

I am trying to do a simple custom size board full of holes for through hole components ( a simple prototyping board) and I am not sure about which is the best way to make the holes.

I have found many resources with totally different answers. For example on this video: https://www.youtube.com/watch?v=s4-Ugi4y9lk (min: 24.00) this guy use the simple command VIA for doing this, but a VIA should be just a connection between layers.  On this discussion How to add connection points for soldered wires , another guy suggest instead the library wirepad.lbr.

This is a working project. not for fun, so I need to be quite sure that I am making the righ hole. Could you someone help me? It will be really appreciate.

  • Sign in to reply
  • Cancel
Parents
  • ardenne
    0 ardenne over 9 years ago

    Thank you all.

    I am not importing nothing from the schematic page because I don't have other components on the board, just holes and a brand logo, so I am making directly the board in the board page of Eagle.

    For a bettere understanding, I am making this simple type of board (see figure below) but with a custom size and a logo.

    Image result for prototyping board

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 9 years ago in reply to ardenne

    It is always best to schematic capture a PCB because it allows revisions and additions to it to be easily accomplished.

    For example - your Proto board - There will most likely be a stage where you want to add power rails or planes to it.

    Facilitating this is done easily using a schematic.

    There's no reason why you can't capture the prototyping area as components and have them placed on your PCB.

    If fact EAGLE works best in this mode because it switches between its schematic and PCB for its Design Rule Checking.

     

    I just kluged this up in moments to illustrate the point. Complete with mounting holes.

    The size of this board is at the maximum freeware limit.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • COMPACT
    0 COMPACT over 9 years ago in reply to ardenne

    It is always best to schematic capture a PCB because it allows revisions and additions to it to be easily accomplished.

    For example - your Proto board - There will most likely be a stage where you want to add power rails or planes to it.

    Facilitating this is done easily using a schematic.

    There's no reason why you can't capture the prototyping area as components and have them placed on your PCB.

    If fact EAGLE works best in this mode because it switches between its schematic and PCB for its Design Rule Checking.

     

    I just kluged this up in moments to illustrate the point. Complete with mounting holes.

    The size of this board is at the maximum freeware limit.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • COMPACT
    0 COMPACT over 9 years ago in reply to COMPACT

    If you look very closely you'll also see the two pads with the enlarged holes as per your photo.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 9 years ago in reply to COMPACT

    It also makes for a good familiarisation practice session with EAGLE for Library, Schematic and PCB editing.