Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Add holes for through hole components
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 7 answers
  • Subscribers 190 subscribers
  • Views 8187 views
  • Users 0 members are here
Related

Add holes for through hole components

ardenne
ardenne over 9 years ago

Hi, I am new in the Eagle world and I am making a 2 layers custom board with Eagle. 

I am trying to do a simple custom size board full of holes for through hole components ( a simple prototyping board) and I am not sure about which is the best way to make the holes.

I have found many resources with totally different answers. For example on this video: https://www.youtube.com/watch?v=s4-Ugi4y9lk (min: 24.00) this guy use the simple command VIA for doing this, but a VIA should be just a connection between layers.  On this discussion How to add connection points for soldered wires , another guy suggest instead the library wirepad.lbr.

This is a working project. not for fun, so I need to be quite sure that I am making the righ hole. Could you someone help me? It will be really appreciate.

  • Sign in to reply
  • Cancel
Parents
  • ardenne
    0 ardenne over 9 years ago

    Ok, so if I have understood well, you suggest me to start with a schematic creating the component "board" and then go into the board page in Eagle.

    I will try to do this. Thank you very much.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ardenne
    0 ardenne over 9 years ago

    Ok, so if I have understood well, you suggest me to start with a schematic creating the component "board" and then go into the board page in Eagle.

    I will try to do this. Thank you very much.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • COMPACT
    0 COMPACT over 9 years ago in reply to ardenne

    Firstly to create a components in a new library by:

    a. defining a package (which just consists of the pads of the size you want),

    b. defining a symbol to associate with the package,

    c. creating a device that correlates the pads of the package with the schematic symbol.

     

    From that create a Project and within that project create a schematic file.

    Place your newly defined device onto your schematic (for a proto board with no connections you won't have to define any nets),

    (I.e. Your schematic will just be a bunch of non-interconnected components)

    Then click the SCH/PCB button and allow EAGLE to create a PCB for you.

     

    Now you can move the device into the position you want on the PCB.

     

    The Schematic and PCB are closely linked allowing you to switch back to the schematic to make changes and by clicking the SCH/PCB button it'll place any new components on the PCB file.

     

    Mechanical holes don't necessarily need to be included on the Schematic and can be placed directly on the PCB.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer