EAGLE User Support (English) Unexpected behavior of EAGLE layout editor
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
  • State Suggested Answer
  • Replies 16 replies
  • Answers 1 answer
  • Subscribers 180 subscribers
  • Views 2709 views
  • Users 0 members are here
  • eagle 6.4.0 professional
  • Layout Editor
Related

Unexpected behavior of EAGLE layout editor

SMD111
SMD111 over 8 years ago

The problem I have is described in the attached images (they are zoom-able).

I have a finalized, fully routed design:

image

At some point I decided to add a new gate to the schematic, so I copy IC5 and paste it as IC9. Please note that no connections on IC9 have been made yet:

image

Simply placing this gate on schematic causes significant changes on the board. As you can see, multiple nets become ripped up, even the nets that have nothing to do with IC5 or IC9.

image

Is it possible to avoid this effect?

Thank you,

Sergey

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 8 years ago

    On 21/07/17 16:35, SMD111 wrote:

    The problem I have is described in the attached images (they are zoom-able).

    I have a finalized, fully routed design:

     

    In what sense is that "fully routed"? The tiny schematic fragment

    clearly shows C5 connected to the power pins of two ICs but on that

    board it's only connected to a jumper. It's blatantly not complete.

     

    At some point I decided to add a new gate to the schematic, so I copy IC5 and paste it as IC9. Please note that no connections on IC9 have been made yet:

    Simply placing this gate on schematic causes significant changes on the board. As you can see, multiple nets become ripped up, even the nets that have nothing to do with IC5 or IC9.

     

    No changes to the board, no nets ripped up, merely the airwires have

    been turned on.

     

    Is it possible to avoid this effect?

     

    Yes, by starting with an actually completely routed board.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 8 years ago

    On 21/07/17 16:35, SMD111 wrote:

    The problem I have is described in the attached images (they are zoom-able).

    I have a finalized, fully routed design:

     

    In what sense is that "fully routed"? The tiny schematic fragment

    clearly shows C5 connected to the power pins of two ICs but on that

    board it's only connected to a jumper. It's blatantly not complete.

     

    At some point I decided to add a new gate to the schematic, so I copy IC5 and paste it as IC9. Please note that no connections on IC9 have been made yet:

    Simply placing this gate on schematic causes significant changes on the board. As you can see, multiple nets become ripped up, even the nets that have nothing to do with IC5 or IC9.

     

    No changes to the board, no nets ripped up, merely the airwires have

    been turned on.

     

    Is it possible to avoid this effect?

     

    Yes, by starting with an actually completely routed board.